Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Interfacing MCUs to external SDRAM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 503 subscribers
  • Views 2239 views
  • Users 0 members are here
  • microcontrollers
Related

Interfacing MCUs to external SDRAM

e14 Contributor
e14 Contributor over 15 years ago

Hi all,

 

I'm looking for a way to interface external SDRAM to MCUs (MCUs having external memory controller / MMU).

I don't know well how drive SDRAM memory (because usually I interface MCUs having RAM internally), but my main problem is external memory terminations.

Please, have anyone explanations, documentation or books titles to address me in solving this issue?

 

Thanks in advance.

Regards.

 

Marco.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hey Marco

    I don't know the specifics of what you doing but a typical approach if your looking for parallel RAM (you can get serial SRAM if access speed isn't a concern) is to select a SRAM, the important parameters being voltage obviously, and then bus width (8/16/32) and access speed.  Then typically you use something like 74HC573 IC's to latch the address from your data bus to the SRAM address pins, using multiple 74HC573's if your bus is bigger than 8 bits.  If you want as fast as possible speed select a MCU with a built in parallel port so the MCU accesses the ram as fast as possible rather than you bit bashing the accesses, but if you don't need get the speed as fast as possible then there's nothing wrong with bit bashing the accesses and your typcailly only talking about a few extra MCU cycles per access.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hey Marco

    I don't know the specifics of what you doing but a typical approach if your looking for parallel RAM (you can get serial SRAM if access speed isn't a concern) is to select a SRAM, the important parameters being voltage obviously, and then bus width (8/16/32) and access speed.  Then typically you use something like 74HC573 IC's to latch the address from your data bus to the SRAM address pins, using multiple 74HC573's if your bus is bigger than 8 bits.  If you want as fast as possible speed select a MCU with a built in parallel port so the MCU accesses the ram as fast as possible rather than you bit bashing the accesses, but if you don't need get the speed as fast as possible then there's nothing wrong with bit bashing the accesses and your typcailly only talking about a few extra MCU cycles per access.