Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Implementation of Neural network (trained in MATLAB) in Microcontroller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 502 subscribers
  • Views 725 views
  • Users 0 members are here
  • microcontollers
  • matlab
  • arm
Related

Implementation of Neural network (trained in MATLAB) in Microcontroller

e14 Contributor
e14 Contributor over 15 years ago

Hi all,

I want to dump my neural network on any controller like PIC AVR or ARM..

I made the network in MATLAB using NFTOOL now,I have simulink file and I want to generate equivalent  "C" code.

and that code compile I want to dump in micro-controller..

I am having Matlab 7.12 R2011a

(Lpcxpresso kit with LPC1114/302 microcontroller

Arduino kit with ATmega 32)

 

Guys.-- Please Help me out....

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hey

     

    I am doing a very similar project. Built a simulink model also using Neural Network Control but am having problems linking my simulink to the Arduino Atmega 2560. Mathworks offers a plugin to allow conversion from the simulink model to a code but i am having problems with it as it only offers 2 board options and the 2560 is not an option. What you can try is the real time workshop function. It takes your simulink model and converts it into a C code.

     

    let me know if this helps or if you find help cause having the same problems and this for my fourth year design project.

     

    Cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hey

     

    I am doing a very similar project. Built a simulink model also using Neural Network Control but am having problems linking my simulink to the Arduino Atmega 2560. Mathworks offers a plugin to allow conversion from the simulink model to a code but i am having problems with it as it only offers 2 board options and the 2560 is not an option. What you can try is the real time workshop function. It takes your simulink model and converts it into a C code.

     

    let me know if this helps or if you find help cause having the same problems and this for my fourth year design project.

     

    Cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dbarne20
    0 dbarne20 over 14 years ago in reply to e14 Contributor

    you can build c code from the model using real time workshop, then simply incorporate the generated c files into a project file and compile via your standard ide / compiler usage.  The advantage seen with boards that are part of the Matlab target support packages is that you can invoke the compiler / create the entire project from the model.  When you use a non-supported target, you have to do a bit more leg work, to bring the auto generated code to the compiled / ready to flash step but it is still a useful tool.