Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Embedded WiFi recommendations?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 2 answers
  • Subscribers 505 subscribers
  • Views 5056 views
  • Users 0 members are here
  • wifi
  • 802.11
  • embedded
  • microcontroller
  • wireless
  • arduino
Related

Embedded WiFi recommendations?

fustini
fustini over 15 years ago

Howdy,

 

I was wondering if anyone might have recommendations for WiFi modules for a low-end embedded system.  I'm primarily thinking of Arduino so a simple interface to the radio would be ideal (not USB).

 

Thanks,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • PBrunner
    PBrunner over 15 years ago in reply to e14 Contributor +1 suggested
    You are perfectly right Julian Freescale has actually 3 different Wifi modules based on 3 different chipsets from 3 different suppliers( http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152106740AFE4…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    There is also TI CC3000 which is a UART-to-WIFI module, probably a more compact solution with respect to the MCW1001A+MRF24WB0Mx couple. Although I've used the Microchip's one in a dev-kit of theirs and…
  • Funklord
    Funklord over 14 years ago +1
    The Microchip MRF24WBOMx modules are great, especially due to the low price, and existing code for 8bit PIC, AVR and Arduino etc. I'm successfully using it with an ATMEGA168 (or better) and WPA2/AES encryption…
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    checkout red pine signals.They have all the documentation along with the module. wifi module can be controlled with AT commands

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    checkout red pine signals.They have all the documentation along with the module. wifi module can be controlled with AT commands

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    I've been using the MRF24WB0MB/RMMRF24WB0MB/RM module from Microchip, together with their TCPIP Stack of course, on a PIC32MX795F512L. If you go down this route, I'd suggest buying a development board to quickly get a demonstration up and going. I've also got a Kinetis K60 tower kit and the AR4100 wifi module, but haven't had the time to do anything with that, so can't give a comparison yet.

     

    For the MRF24W modules, they quote 154mA when TX is on @ 0dB. I'm using an SD card and GPS as well, seeing about 230mA total draw, everything on, with the above PIC32 MCU. I've found the examples fairly easy to modify and have managed to write my own AJAX code to handle button pushes etc. The example code polls for the LEDs & buttons @ 100Hz so will use more power than button pushes sending status / update requests when pushed.

     

    You might also like to check out the WizFi 210 as a serial interfaced module - again I've yet to evaluate this but it's on my desk!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to e14 Contributor

    Thanks for the input from everyone.  I ended up ordering the WiFly shield from SparkFun although I wish I would have pursued the Microchip module.

     

    At the time, I was in a big rush to have a basic prototype working and the shield seemed like the quickest route.  However, since the Roving Network's WiFly module has no SPI interface, the shield adds a UART to SPI bridge chip so that the Arduino's single UART is spared.

     

    In theory this sounds good, but I have found it introduced extra complexity in troubleshooting my code.  I found it very hard to implement the seemingly simple functionality I needed from the WiFly: associate, connect, GET a URL that returns small amount  of text, sleep for 5 min, repeat.

     

    At $90, I don't think the shield was a good buy and would prefer module with SPI.  I found an ATMega328 board called the Yellow Jacket with the latest Microchip module for $55 from Rugged Circuits. Great deal as module is $30 and don't think I could solder it's smaller pitch.  I am waiting for it to be back in stock - Rugged Circuits told me there is a world wide shortage of the Microchip part.

     

    Thanks,

    Drew