Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Embedded WiFi recommendations?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 2 answers
  • Subscribers 505 subscribers
  • Views 5033 views
  • Users 0 members are here
  • wifi
  • 802.11
  • embedded
  • microcontroller
  • wireless
  • arduino
Related

Embedded WiFi recommendations?

fustini
fustini over 15 years ago

Howdy,

 

I was wondering if anyone might have recommendations for WiFi modules for a low-end embedded system.  I'm primarily thinking of Arduino so a simple interface to the radio would be ideal (not USB).

 

Thanks,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • PBrunner
    PBrunner over 15 years ago in reply to e14 Contributor +1 suggested
    You are perfectly right Julian Freescale has actually 3 different Wifi modules based on 3 different chipsets from 3 different suppliers( http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152106740AFE4…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    There is also TI CC3000 which is a UART-to-WIFI module, probably a more compact solution with respect to the MCW1001A+MRF24WB0Mx couple. Although I've used the Microchip's one in a dev-kit of theirs and…
  • Funklord
    Funklord over 14 years ago +1
    The Microchip MRF24WBOMx modules are great, especially due to the low price, and existing code for 8bit PIC, AVR and Arduino etc. I'm successfully using it with an ATMEGA168 (or better) and WPA2/AES encryption…
Parents
  • Funklord
    0 Funklord over 14 years ago

    The Microchip MRF24WBOMx modules are great, especially due to the low price, and existing code for 8bit PIC, AVR and Arduino etc.

    I'm successfully using it with an ATMEGA168 (or better) and WPA2/AES encryption.

    You do NOT need MCW1001A or any other chip to control it, an 8bit micro with around 6k flash to spare is enough.

     

    They can be gotten for around 17eur/each @100pcs here:

    http://se.mouser.com/Search/Refine.aspx?Keyword=mrf24wbom

    Although they are probably cheaper from microchip direct.

     

    I believe the original designer is Gainspan, but I'm not sure.

     

    A while ago, I had a few small breakout boards fabricated for connecting a MRF24WBOMx to SPI with a single 9 pin 2.54mm header... interrupts (optional) and such are broken out.

    If anyone is interested, I have a few extra boards I could send.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to Funklord

    Thanks for the tip.  I'm going to be returning to my wifi project in a little bit with the aim of building about 10 devices which display calendar meeting status on an LCD.  I'll be looking to make a design with minimal cost so the WiFly shield I had been using is definitely out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fustini
    0 fustini over 14 years ago in reply to Funklord

    Thanks for the tip.  I'm going to be returning to my wifi project in a little bit with the aim of building about 10 devices which display calendar meeting status on an LCD.  I'll be looking to make a design with minimal cost so the WiFly shield I had been using is definitely out.