Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Confused with headerfiles and undefined names
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 502 subscribers
  • Views 363 views
  • Users 0 members are here
  • p18f458
  • header
  • Cube
  • led
  • define
  • mcu
  • bitnames
Related

Confused with headerfiles and undefined names

e14 Contributor
e14 Contributor over 15 years ago

Hello,

 

I'm working on my LED cube but have come across a problem.

 

I'm programming in C with MPLAB, C18 compiler and the P18F458 MCU.

 

I have included the headerfile of the MCU with: #include <p18f458.h>

 

After writing a piece of code, I get some errors about undefined symbols.

 

names like PORTA, TRISA work normal but bitnames don't work.


when I try to use bitnames to control timers, ports etc the compiler gives an error.

 

C:\Programmeren\Project_LEDcube\Software\Cube_Main_16082011\src\Main.c:61:Error [1105] symbol 'RE0' has not been defined

 

I do not understand why symbols like PORTE work and RE0 not, they are from the same headerfile if I'm right?

 

hope someone can help,

 

Futience

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    After some try and error I have found a solution. I searched in the C18 userguide and found out that in stead of working with the symbol "RE0" I have to use "PORTEbits.RE0"
    I wasn't used to do it this way but it seems to work. Is there a simple way to convert this headerfile so I can use only "RE0" ???

     

    Futience

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    After some try and error I have found a solution. I searched in the C18 userguide and found out that in stead of working with the symbol "RE0" I have to use "PORTEbits.RE0"
    I wasn't used to do it this way but it seems to work. Is there a simple way to convert this headerfile so I can use only "RE0" ???

     

    Futience