Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Does any one know of a USB to TTL (5v) converter?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 502 subscribers
  • Views 853 views
  • Users 0 members are here
Related

Does any one know of a USB to TTL (5v) converter?

SGarciaV
SGarciaV over 14 years ago

Hi all, I have a friend that is looking for a board (or product) that can connect to the USB port and have 4 to 8 TTL (5v) outputs. Although inputs are not strictly necessary, if the item has these it would be of interest. He hopes to find something in the $50 range.

 

He mentions that he is looking to control external devices (lamps, motors, buzzers, etc.) through the USB port. He is looking for the TTL outputs and will develop his own interface electronics (opto coupler, triac, etc.) that will use the TTL signals as inputs.

 

Does any one have any suggestions?

 

If this is not the best group to ask this, please let me know and I'll repost in the recommended group. Thanks! Salvador

  • Sign in to reply
  • Cancel
  • YT2095
    0 YT2095 over 14 years ago

    Probably the easiest way would be through an FTDI board (or any USB to serial converter) and then use a simple microcontroller, even an arduino will do this task easily of taking in serial data, and outputting this as Binary.

    USB to Parallel port devices are easy to come by also.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to YT2095

    Yeah, I think any microcontroller dev board with USB interface (or external FTDI interface) would fit this requirement like Arduino, Propeller, etc.  An alternative may be to get an explicit USB controller board like this Velleman kit (which I've seen at RadioShack):

     

    http://www.velleman.eu/products/view/?country=be&lang=en&id=351346

     

    It has a Windows interface and also now works with Android & iOS.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Catwell
    0 Catwell over 14 years ago

    Salvador,

     

    Easiest to do is get a USB to serial/TTL breakout board.USB to serial/TTL breakout board.

     

    Or you can build one yourself:

    image

    This is taken from Ben Lennard's website.

     

    Good luck.

     

    Cabe

    http://twitter.com/Cabe_e14
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 14 years ago

    YT2095, Fustin and Cabe: Thanks for your replies. I have passed a link to this thread to my friend, hoping that he finds this information useful. Love the build your own option! Regards, Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 14 years ago

    Thank you all for your help. My friend Tony is located in Mexico and sends this message:

     

    "Muchas gracias por la búsqueda, por favor manda mis agradecimientos  a tus compañeros del web."

     

    Saludos.

     

    Antonio Hernández Cárdenas

     

    Translated: "Thanks for doing the search, please pass on my gratefulness to you colleagues on the Web."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MicrochipRTCfr
    0 MicrochipRTCfr over 14 years ago in reply to SGarciaV

    Hi,

     

    There are also other very cheap alternatives :

     

    1/ MCP2200

    It is a UART <==> USB bridge with 8 I/Os and  E2PROM.

    You can find here a schematic (just remove the MAX232 chip which you don't need

    this device is seen as a COM port (USB CDC class)

     

    2/ HEXWAX

    This company develops very nice devices that connect to PC via USB using the HID class (no DRIVER needed).

     

    regards