Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Does any one know of a USB to TTL (5v) converter?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 502 subscribers
  • Views 864 views
  • Users 0 members are here
Related

Does any one know of a USB to TTL (5v) converter?

SGarciaV
SGarciaV over 14 years ago

Hi all, I have a friend that is looking for a board (or product) that can connect to the USB port and have 4 to 8 TTL (5v) outputs. Although inputs are not strictly necessary, if the item has these it would be of interest. He hopes to find something in the $50 range.

 

He mentions that he is looking to control external devices (lamps, motors, buzzers, etc.) through the USB port. He is looking for the TTL outputs and will develop his own interface electronics (opto coupler, triac, etc.) that will use the TTL signals as inputs.

 

Does any one have any suggestions?

 

If this is not the best group to ask this, please let me know and I'll repost in the recommended group. Thanks! Salvador

  • Sign in to reply
  • Cancel
Parents
  • SGarciaV
    0 SGarciaV over 14 years ago

    Thank you all for your help. My friend Tony is located in Mexico and sends this message:

     

    "Muchas gracias por la búsqueda, por favor manda mis agradecimientos  a tus compañeros del web."

     

    Saludos.

     

    Antonio Hernández Cárdenas

     

    Translated: "Thanks for doing the search, please pass on my gratefulness to you colleagues on the Web."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MicrochipRTCfr
    0 MicrochipRTCfr over 14 years ago in reply to SGarciaV

    Hi,

     

    There are also other very cheap alternatives :

     

    1/ MCP2200

    It is a UART <==> USB bridge with 8 I/Os and  E2PROM.

    You can find here a schematic (just remove the MAX232 chip which you don't need

    this device is seen as a COM port (USB CDC class)

     

    2/ HEXWAX

    This company develops very nice devices that connect to PC via USB using the HID class (no DRIVER needed).

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • MicrochipRTCfr
    0 MicrochipRTCfr over 14 years ago in reply to SGarciaV

    Hi,

     

    There are also other very cheap alternatives :

     

    1/ MCP2200

    It is a UART <==> USB bridge with 8 I/Os and  E2PROM.

    You can find here a schematic (just remove the MAX232 chip which you don't need

    this device is seen as a COM port (USB CDC class)

     

    2/ HEXWAX

    This company develops very nice devices that connect to PC via USB using the HID class (no DRIVER needed).

     

    regards