Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Microcontrollers, SoC's, CPU's, ARM and programming of those things
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 502 subscribers
  • Views 2718 views
  • Users 0 members are here
  • test
  • jtag
  • soc
  • ieee_1149.1
  • computer
  • programming
  • embedded
  • operating_system
  • microcontroller
  • cpu
  • arm
Related

Microcontrollers, SoC's, CPU's, ARM and programming of those things

sinistra92
sinistra92 over 14 years ago

Hello everyone,

 

Up to now, I have been programming 8 bit AVRs (in C). I now ordered Raspberry Pi and I want to switch on to a little more advanced chips (eg. ARM in RPi and AVR32).

I have trouble understanding how all the "more advanced" chips work and how they are programmed.

 

This is what I know (or I think is true):

I know that to get a microcontroller to work, I need to write a program on the computer and program the device through a programmer.

This also applies to 32-bit microcontrollers (many of which are ARM based). In this case, apart of boot-loading or company specific port, only JTAG would program the device.

ARM is just an architecture, or a "template" to some extend, that gives base to uC's and so there are many different companies making their 32bit around ARM.

Above ARM and 32 bit uC are Embedded solutions, eg. SoC's which are a composition of at least one microcontroller inside (commonly ARM), some flash, RAM, ROM, GPU optionally, etc.

SoC's are good to run a simple OS like Linux. A GPU is a separately programmable part of an SoC.

CPU is not a microntroller, is very fast and does the instructions which are given it.

JTAG is a universal device that can debug and programm all JTAG supportive devices, given I have appropriate software.

 

 

Now things I don't understand:

SoC's have a microcontroller inside them, so they must be programmable, but are they all like that? Does an SoC have a program stored in it's flash, that it fetches instructions from, just like an 8bit?

Something must take files from an SD card and run them in a Raspberry Pi, something must tell the GPU inside what display interface to use etc, but I can't find a source code, or an evidence of a program being run inside a SoC.

How is it really happening? (1)

 

About CPUs, I think they are not programmable, so they are supported by BIOS that fetches the initial instructions from HDD boot section and the CPU automatically performs all what is given to it, and so, the motherboard has to take care of all the results the CPU "throws out".

Is this really what is happening? (2)

 

About JTAG. It is mainly a test solution for debugging etc, but one of its uses is accessing the memories of a micronotroller, so they can be therefore programmed. But then why are there so many different JTAGs on the market?

Why isn't one JTAG IEEE 1149.1 compatible with ALL the chips? The instructions are universal, aren't they? Why is there a special JTAG for AVR32 and a different one for Xilinx? (3)

 

 

I am sorry to ask so many questions, but I really couldn't find very much information about those and I think a discussion like this would help people by bringing these answers in one place. I have numbered three distinct issues.

If there is something I misunderstand in the first part, please tell me as it may be trivial to some people, but not as such to me.

 

 

Thanks,

Wojciech

  • Sign in to reply
  • Cancel

Top Replies

  • Kelv
    Kelv over 14 years ago +2 suggested
    ok, please remember this reply is all generic SoC, if you would like to send me your Pi I will be happy to look further into it for you 1+2) Whilst I can't comment on the boot process of the Pi, generally…
  • e14 Contributor
    e14 Contributor over 14 years ago +2 suggested
    About question 2: Here is what I can tell you: Yes, a CPU performs what it is given to it... To do so, it has registers witch are small blocks of real physical memory in the CPU. The quantity varies with…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    1) as far as I know there is a bootloader in there. It may be configurable or not, this is the decision of the product manufacturer. In the case of the Raspi it is not: it's hardcoded to load from the…
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    About what a CPU executes when the power is turned on, I'm not sure, I will let somebody else answer this question. From what I remember, it goes executes the instruction to a specific address (that is not 0x00000000)...

     

    As for your edit on FT2232H:

    To know what is devices are compatible with your board, I would look at these first:

    • On their TIAO's wiki:http://www.tiaowiki.com/w/TIAO_USB_Multi_Protocol_Adapter_User's_Manual
    • in OpenOCD documentation: http://openocd.sourceforge.net/doc/html/Debug-Adapter-Hardware.html#Debug-Adapter-Hardware
    • and on FTDI's website : http://www.ftdichip.com/Products/ICs/FT2232H.htm

     

    You will find that with TIAO's board, beacuse of the FT2232H, you can do more than just JTAG. I use a similar IC in one of my projects (a FT232H), so the EEPROM they are talking about is on FTDI's web site. Browse a bit, they have a software that you need to download. This software allows you to program the EEPROM  so that you can change the type of conversion the device does : USB to I2C, USB to SPI.... Also, they have "application notes" that tells you how to do it, what to do and so forth....

     

    And to answer you question: I don't know if you can program *any* devices but It would be safe to say "most devices"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sinistra92
    0 sinistra92 over 14 years ago in reply to e14 Contributor

    Yes, I looked at most of the stuff, although most of it isn't helpful.

     

    This shows:

    http://www.youtube.com/watch?v=rnukKDyj4LI

    that FT2232 can program LPC176x devices (using OOCD), so at least I can play with those for now.

     

    I am not sure, but it seems that the biggest problem is to get the right support on the computer side for the chip, as the jtag itself is flexible for many of them.  Once I get my TUMPA (shipped from Canada to UK) and a few ARM or AVR32 or others, I'll post around.

    I was really confused about all this JTAG thing, because I thought since it doesn't say in datasheet of a device it can be programmed by JTAG, then it couldn't. Apparently it often is not the case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sinistra92
    0 sinistra92 over 14 years ago in reply to e14 Contributor

    Yes, I looked at most of the stuff, although most of it isn't helpful.

     

    This shows:

    http://www.youtube.com/watch?v=rnukKDyj4LI

    that FT2232 can program LPC176x devices (using OOCD), so at least I can play with those for now.

     

    I am not sure, but it seems that the biggest problem is to get the right support on the computer side for the chip, as the jtag itself is flexible for many of them.  Once I get my TUMPA (shipped from Canada to UK) and a few ARM or AVR32 or others, I'll post around.

    I was really confused about all this JTAG thing, because I thought since it doesn't say in datasheet of a device it can be programmed by JTAG, then it couldn't. Apparently it often is not the case.