Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Microcontrollers, SoC's, CPU's, ARM and programming of those things
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 502 subscribers
  • Views 2718 views
  • Users 0 members are here
  • test
  • jtag
  • soc
  • ieee_1149.1
  • computer
  • programming
  • embedded
  • operating_system
  • microcontroller
  • cpu
  • arm
Related

Microcontrollers, SoC's, CPU's, ARM and programming of those things

sinistra92
sinistra92 over 14 years ago

Hello everyone,

 

Up to now, I have been programming 8 bit AVRs (in C). I now ordered Raspberry Pi and I want to switch on to a little more advanced chips (eg. ARM in RPi and AVR32).

I have trouble understanding how all the "more advanced" chips work and how they are programmed.

 

This is what I know (or I think is true):

I know that to get a microcontroller to work, I need to write a program on the computer and program the device through a programmer.

This also applies to 32-bit microcontrollers (many of which are ARM based). In this case, apart of boot-loading or company specific port, only JTAG would program the device.

ARM is just an architecture, or a "template" to some extend, that gives base to uC's and so there are many different companies making their 32bit around ARM.

Above ARM and 32 bit uC are Embedded solutions, eg. SoC's which are a composition of at least one microcontroller inside (commonly ARM), some flash, RAM, ROM, GPU optionally, etc.

SoC's are good to run a simple OS like Linux. A GPU is a separately programmable part of an SoC.

CPU is not a microntroller, is very fast and does the instructions which are given it.

JTAG is a universal device that can debug and programm all JTAG supportive devices, given I have appropriate software.

 

 

Now things I don't understand:

SoC's have a microcontroller inside them, so they must be programmable, but are they all like that? Does an SoC have a program stored in it's flash, that it fetches instructions from, just like an 8bit?

Something must take files from an SD card and run them in a Raspberry Pi, something must tell the GPU inside what display interface to use etc, but I can't find a source code, or an evidence of a program being run inside a SoC.

How is it really happening? (1)

 

About CPUs, I think they are not programmable, so they are supported by BIOS that fetches the initial instructions from HDD boot section and the CPU automatically performs all what is given to it, and so, the motherboard has to take care of all the results the CPU "throws out".

Is this really what is happening? (2)

 

About JTAG. It is mainly a test solution for debugging etc, but one of its uses is accessing the memories of a micronotroller, so they can be therefore programmed. But then why are there so many different JTAGs on the market?

Why isn't one JTAG IEEE 1149.1 compatible with ALL the chips? The instructions are universal, aren't they? Why is there a special JTAG for AVR32 and a different one for Xilinx? (3)

 

 

I am sorry to ask so many questions, but I really couldn't find very much information about those and I think a discussion like this would help people by bringing these answers in one place. I have numbered three distinct issues.

If there is something I misunderstand in the first part, please tell me as it may be trivial to some people, but not as such to me.

 

 

Thanks,

Wojciech

  • Sign in to reply
  • Cancel

Top Replies

  • Kelv
    Kelv over 14 years ago +2 suggested
    ok, please remember this reply is all generic SoC, if you would like to send me your Pi I will be happy to look further into it for you 1+2) Whilst I can't comment on the boot process of the Pi, generally…
  • e14 Contributor
    e14 Contributor over 14 years ago +2 suggested
    About question 2: Here is what I can tell you: Yes, a CPU performs what it is given to it... To do so, it has registers witch are small blocks of real physical memory in the CPU. The quantity varies with…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    1) as far as I know there is a bootloader in there. It may be configurable or not, this is the decision of the product manufacturer. In the case of the Raspi it is not: it's hardcoded to load from the…
Parents
  • sinistra92
    0 sinistra92 over 14 years ago

    Riiiiight...

     

    Thank you very much guys, I understand a lot more now.

     

    >Kelv:

    So if a manufaturer makes a read-only bootrstrap section, then the cpu looks for the binaries always in the same place (as it appears to be with RPi: it always looks for kernel.img on the memory card and runs it) but the manufacturer probably doesn't disclose what bootstrap there is, unless to professional designers, I guess (requiring NDA). In programmable cases we could write our own, or just make a program that would go to the flah straight in.

     

    Then the software difference between a SoC and a normal 32bit microcontroller is mainly the fact that instead of having all the program in their flash memory, they use bootloader to download (or run straight) from external memory, eg. SD. Am I more or less right?

    If so, then I suppose that the bootloader is a lot smaller comparing to a typical ARM flash memory, not in a SoC.

     

     

    >Nicolas:

    In a case you described, what is the first thing that loads the first instruction from memory (HDD bootloader section, I presume) into CPU working registers? Is it BIOS?

    Or does the CPU have an initial algorith-like sequence that fetches the first instructions?

     

     

    Thanks,

    Wojciech

     

    Edit:

     

    Ah, one more thing:

    I got myself the FT2232H USB to JTAG adapter (a while ago, now), which is said to be working well with OOCD.

    Now, how do I know what devices are compatible with this adapter, as no-one actually says that their microcontroller only accepts such vid's and pid's?

    I assume it is the jtag device (adapter) that has to be compatible with the uC, not debugger running on computer.

    The board I have is called TIAO USB Multi-Protocol Adapter (TUMPA)and it is claimed to have an eeprom that can be programmed with own vendor and product ID's.

    Does that mean It can program any device?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sinistra92
    0 sinistra92 over 14 years ago

    Riiiiight...

     

    Thank you very much guys, I understand a lot more now.

     

    >Kelv:

    So if a manufaturer makes a read-only bootrstrap section, then the cpu looks for the binaries always in the same place (as it appears to be with RPi: it always looks for kernel.img on the memory card and runs it) but the manufacturer probably doesn't disclose what bootstrap there is, unless to professional designers, I guess (requiring NDA). In programmable cases we could write our own, or just make a program that would go to the flah straight in.

     

    Then the software difference between a SoC and a normal 32bit microcontroller is mainly the fact that instead of having all the program in their flash memory, they use bootloader to download (or run straight) from external memory, eg. SD. Am I more or less right?

    If so, then I suppose that the bootloader is a lot smaller comparing to a typical ARM flash memory, not in a SoC.

     

     

    >Nicolas:

    In a case you described, what is the first thing that loads the first instruction from memory (HDD bootloader section, I presume) into CPU working registers? Is it BIOS?

    Or does the CPU have an initial algorith-like sequence that fetches the first instructions?

     

     

    Thanks,

    Wojciech

     

    Edit:

     

    Ah, one more thing:

    I got myself the FT2232H USB to JTAG adapter (a while ago, now), which is said to be working well with OOCD.

    Now, how do I know what devices are compatible with this adapter, as no-one actually says that their microcontroller only accepts such vid's and pid's?

    I assume it is the jtag device (adapter) that has to be compatible with the uC, not debugger running on computer.

    The board I have is called TIAO USB Multi-Protocol Adapter (TUMPA)and it is claimed to have an eeprom that can be programmed with own vendor and product ID's.

    Does that mean It can program any device?