Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum STM32F2 LSE RTC crystal issue: Can anyone help?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 502 subscribers
  • Views 2019 views
  • Users 0 members are here
  • crystal
  • clock
  • lse
  • uc
  • controller
  • ppm
  • rtc
  • stm32
  • 32.768khz
  • stm32f2
  • st
Related

STM32F2 LSE RTC crystal issue: Can anyone help?

e14 Contributor
e14 Contributor over 13 years ago

Hello

 

We use the STM32F2 for a project and have problems with the LSE crystal.

 

We use a Citizen CMR200T32.768KDZF-UTCMR200T32.768KDZF-UT crystal (32.768kHz, CL=6pF, Farnell Nr. 1652560) wich has a gain margin of 6.1 (according to the ST application note AN2867) and therefore is suitable.

 

It worked fine with STM32F205VGT6 Ref Y, now we changed to Ref X and the frequency shifts about 40ppm! There are no information about changes made from Ref Y to Ref X (despite other bootloader version).

 

With uC Ref Y: f=32.7679kHz (-3ppm)

With uC Ref X: f=32.7694kHz (+43ppm)

 

The measurement are made with the same layout, crystal and CL1/CL1 of 4.7pF, only the uC has changed. The frequency is measured at PA8 which outputs the clock trough microcontroller clock output (MCO1).

 

 

Can anyone help? How can we build a accurate RTC when the frequency shifts from uC to uC?

 

Regards,

Timon

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    How many board been tested?  I have designed a board, it have similar problem.  I found the reasons are bad layout and bad soldering. Hope my experience is usefull for you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    @Tech_Support: I've seen this errata but thing this has nothing to do with my problem. It's for the HSE and also the STM32F205 doesn't has ethernet.

     

    @Zhi Deng: Yes, we have testet several boards, some hand soldered some reflow soldered. They all show the same problem.

     

    I'm in contact with ST and they said it's a well known problem but they havn't a solution..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    "they havn't a solution" ?  Quite a bad news.

    Solution 1: If  you must use this MCU and RTC, you can use a wrong CL(Attempt various kinds of values). But i dont recommend this solution.

    Solution 2 : Add a external RTC IC, eg: DS1302, PCF8563 . i think this solution is a good choice.

    Solution 3: Cry with your boards, and wait for ST repair the issue.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    "they havn't a solution" ?  Quite a bad news.

    Solution 1: If  you must use this MCU and RTC, you can use a wrong CL(Attempt various kinds of values). But i dont recommend this solution.

    Solution 2 : Add a external RTC IC, eg: DS1302, PCF8563 . i think this solution is a good choice.

    Solution 3: Cry with your boards, and wait for ST repair the issue.image