Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum WHICH MICROCONTROLLER DO I CHOOSE?? :/
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 503 subscribers
  • Views 1085 views
  • Users 0 members are here
Related

WHICH MICROCONTROLLER DO I CHOOSE?? :/

e14 Contributor
e14 Contributor over 12 years ago

Hey All,

 

I'm working on this board which will bridge WIFI to Bluetooth Smart and I've decided pretty much on all the components except the microcontroller image image! I 've been contemplating on this for quite sometime and i could use some help in shortlisting/ finalizing on the microcontroller which could handly both (WIFI and BLE) the stacks and ya..it would help if the microcontroller is as cheap as it can get probably around 5$ or so. Kindly help me out.

The minimum specifications i would like to have on the uC would be:

1. 64 Kb Flash

2. 16 Kb RAM

3. 1Kb EEPROM (optional)

4. USB 2.0  pins (Can probably leave it out if it influences cost a lot)

5. I2C/SPI/UART

6. UltraLowpower

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Kinetis K20 (Cortex M4) has a 32k on-chip EEPROM available: NXP Freedom Development Platform for the Kinetis K20 USB MCUs

    Kinetis KL26 is very low power (Cortex M0+) and has all the other features you're looking for, probably the more interesting one for you due to lower power: Freedom Development Platform for Kinetis KL16 and KL26 MCUs (up to 128 KB Flash)

     

    Both chips are around $2-$2.50 in large quantities.

     

    http://mcuoneclipse.com/2013/02/14/bluetooth-with-the-freedom-board/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Kinetis K20 (Cortex M4) has a 32k on-chip EEPROM available: NXP Freedom Development Platform for the Kinetis K20 USB MCUs

    Kinetis KL26 is very low power (Cortex M0+) and has all the other features you're looking for, probably the more interesting one for you due to lower power: Freedom Development Platform for Kinetis KL16 and KL26 MCUs (up to 128 KB Flash)

     

    Both chips are around $2-$2.50 in large quantities.

     

    http://mcuoneclipse.com/2013/02/14/bluetooth-with-the-freedom-board/