Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum WHICH MICROCONTROLLER DO I CHOOSE?? :/
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 503 subscribers
  • Views 1081 views
  • Users 0 members are here
Related

WHICH MICROCONTROLLER DO I CHOOSE?? :/

e14 Contributor
e14 Contributor over 12 years ago

Hey All,

 

I'm working on this board which will bridge WIFI to Bluetooth Smart and I've decided pretty much on all the components except the microcontroller image image! I 've been contemplating on this for quite sometime and i could use some help in shortlisting/ finalizing on the microcontroller which could handly both (WIFI and BLE) the stacks and ya..it would help if the microcontroller is as cheap as it can get probably around 5$ or so. Kindly help me out.

The minimum specifications i would like to have on the uC would be:

1. 64 Kb Flash

2. 16 Kb RAM

3. 1Kb EEPROM (optional)

4. USB 2.0  pins (Can probably leave it out if it influences cost a lot)

5. I2C/SPI/UART

6. UltraLowpower

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Towards the end of the article it says that it can be used only for programmin but not for debugging. image do you have any other suggestions other than Freescale microcontrollers?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Towards the end of the article it says that it can be used only for programmin but not for debugging. image do you have any other suggestions other than Freescale microcontrollers?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    Why not use an ST ARM based micro - lots of cheap dev kits and cheap (STLINK) debugger

     

     

    STMICROELECTRONICS - ST-LINK/V2 - ICD/PROGRAMMER, FOR STM8, STM32

     

     

    STMICROELECTRONICSST-LINK/V2
    Image is for illustrative purposes only.
    Please refer to product description

     

     

    Manufacturer:
    STMICROELECTRONICS
    Order Code:
    1892523
    Manufacturer Part No:
    ST-LINK/V2

     

    Technical Data Sheet (94.02KB) EN
    Technical Data Sheet (94.02KB) EN

    image

     

    You can use the free version of the Keil/ARM tools.
    MK

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 12 years ago in reply to michaelkellett

    Thanks Michael, can you please suggest a part from ST which adheres to the above specs.

    I have been looking into the ST M0+ portfolio and none of those were capable enough.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to gsgill112

    STM32 32-bit ARM Cortex MCUs - STMicroelectronics

     

    MK