Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum FTDI - DB9-USB-D3-F - MODULE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 1585 views
  • Users 0 members are here
  • usb/rs232
  • ft232r
  • ftdi
Related

FTDI - DB9-USB-D3-F - MODULE

vivi
vivi over 11 years ago

Hello everybody,

have you anyone used DB9-USB-D3-F - FTDI - MODULE, USB TO UART, 1 CH, FT232R | Farnell ? I need them as USB/RS232 converters.. I have bought two modules, but I cant send any data into PC from any of them. If I connect logic analyzer to TXD pin, so I can send data from PC terminal to "logic analyzer" (so FTDI driver should be OK). But when I connect RX to TX (to make a loop), so transmitted data never come back to terminal. I have WIN7.

 

Thanks for any idea..

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to vivi +1
    It looks as if you are up and running now - great. I used to work with an engineer who wouldn't bother to to specify RX and TX because he said that in on average least 50% of cases someone would make a…
Parents
  • vivi
    0 vivi over 11 years ago

    I have tried it on three various computers with various terminal programs, always the same result. I have tried to use RTS/CTS, but no progress. In datasheet is written, that this module can work without flow control (the same information is written in FT232R datasheet as well).

     

    If I connect to PC ordinary RS232 cabel, connect Rx to Tx (to make a loop) so every sent data are immediately looped back to Rx window in terminal (without any RTS/CTS etc... signals). It seems, that I have bought corrupted modules. But It is strange, two new modules and both do not work..

     

    Thank for your comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to vivi

    vivi wrote:

     

    If I connect to PC ordinary RS232 cable, connect Rx to Tx (to make a loop) so every sent data are immediately looped back to Rx window in terminal (without any RTS/CTS etc... signals). It seems, that I have bought corrupted modules. But It is strange, two new modules and both do not work..

    If I understand this correctly, you have connected a standard RS-232 cable to a PC's serial port and you can loop back RXD to TXD with no problem.  (Must be an old PC image)

     

    In this case, it could be a problem with the Windows driver.  I don't know how to fix Windows drivers problems, but this might be worth searching.  FTDI's site www.ftdichip.com might have some driver-related documents that could help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to vivi

    vivi wrote:

     

    If I connect to PC ordinary RS232 cable, connect Rx to Tx (to make a loop) so every sent data are immediately looped back to Rx window in terminal (without any RTS/CTS etc... signals). It seems, that I have bought corrupted modules. But It is strange, two new modules and both do not work..

    If I understand this correctly, you have connected a standard RS-232 cable to a PC's serial port and you can loop back RXD to TXD with no problem.  (Must be an old PC image)

     

    In this case, it could be a problem with the Windows driver.  I don't know how to fix Windows drivers problems, but this might be worth searching.  FTDI's site www.ftdichip.com might have some driver-related documents that could help.