Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum FTDI - DB9-USB-D3-F - MODULE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 504 subscribers
  • Views 1581 views
  • Users 0 members are here
  • usb/rs232
  • ft232r
  • ftdi
Related

FTDI - DB9-USB-D3-F - MODULE

vivi
vivi over 11 years ago

Hello everybody,

have you anyone used DB9-USB-D3-F - FTDI - MODULE, USB TO UART, 1 CH, FT232R | Farnell ? I need them as USB/RS232 converters.. I have bought two modules, but I cant send any data into PC from any of them. If I connect logic analyzer to TXD pin, so I can send data from PC terminal to "logic analyzer" (so FTDI driver should be OK). But when I connect RX to TX (to make a loop), so transmitted data never come back to terminal. I have WIN7.

 

Thanks for any idea..

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to vivi +1
    It looks as if you are up and running now - great. I used to work with an engineer who wouldn't bother to to specify RX and TX because he said that in on average least 50% of cases someone would make a…
Parents
  • vivi
    0 vivi over 11 years ago

    I have tried it on three various computers with various terminal programs, always the same result. I have tried to use RTS/CTS, but no progress. In datasheet is written, that this module can work without flow control (the same information is written in FT232R datasheet as well).

     

    If I connect to PC ordinary RS232 cabel, connect Rx to Tx (to make a loop) so every sent data are immediately looped back to Rx window in terminal (without any RTS/CTS etc... signals). It seems, that I have bought corrupted modules. But It is strange, two new modules and both do not work..

     

    Thank for your comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to vivi

    Can you draw a little diagram of your set up - I don't understand at all where the RS232 cable comes into things.

    Remember the FTDI module you have is NOT RS232 - it converts USB into logic level NRZ (or Uart type) comms. It will not work with RS232 signal levels.

    There are several settings in Windows for the FTDI chip driver. Can you tell us which terminal program you are using ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to vivi

    Can you draw a little diagram of your set up - I don't understand at all where the RS232 cable comes into things.

    Remember the FTDI module you have is NOT RS232 - it converts USB into logic level NRZ (or Uart type) comms. It will not work with RS232 signal levels.

    There are several settings in Windows for the FTDI chip driver. Can you tell us which terminal program you are using ?

     

    MK