Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum WHAT MCU PROGRAMERS DO YOU USE.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 504 subscribers
  • Views 1801 views
  • Users 0 members are here
  • programer
  • mcu
Related

WHAT MCU PROGRAMERS DO YOU USE.

supper_slash
supper_slash over 12 years ago

Being new to Micro-controllers, i was wanting to know what i should do to start off with as far as programers.

I am thinking PIC programers would be the best option, because of the PIC selection, but i don't know if that is a good idea.

For example, can a pic 3 Programer program ALL Pic chips, or are there limitations?  I made a mistake in buying a MSP 430 Launchpad, and although it works fine, i have a hard time figuring out what it can program, and can not program. Some chips it has listed as being able to program, i can not get it to access, and so it ended up being a wast, and at the same time, i have not yet figured out what programer Texas instrument has that will program there chips, like the pic3 programer. So, is there a couple of programmers that you all have that covers most of all of your needs? Atmel, Pic, TI, And any others? 

What do you use?

I don't haft to use pic, in fact i have never used pic, so, i am completely open to pros, and cons, and suggestions.

I just need a broad range, from 8-40 pin applications, through hole use primarily. I need to program the chip, and than place it on a board, and leave it.


Please feel free to give any ideas, or advice.  Thank-you in advance.


  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    There are lots of microcontroller development boards that include a USB programmer.  Having a separate "MCU programmer" is not that relevant these days.  The $4 PSoC 4 boards that Douglas mentions are very attractive, except that PSoC Creator only runs on Windows.  ST has a nice series of STM Discovery boards that use the same ST-LINK programmer, which is included on the boards.  There are also a number of boards that support ARM mbed which looks like an easy way to program MCUs.

     

    I suggest choosing an MCU family you link -- the choice of programmers will be clear.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago

    There are lots of microcontroller development boards that include a USB programmer.  Having a separate "MCU programmer" is not that relevant these days.  The $4 PSoC 4 boards that Douglas mentions are very attractive, except that PSoC Creator only runs on Windows.  ST has a nice series of STM Discovery boards that use the same ST-LINK programmer, which is included on the boards.  There are also a number of boards that support ARM mbed which looks like an easy way to program MCUs.

     

    I suggest choosing an MCU family you link -- the choice of programmers will be clear.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer