Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum WHAT MCU PROGRAMERS DO YOU USE.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 504 subscribers
  • Views 1800 views
  • Users 0 members are here
  • programer
  • mcu
Related

WHAT MCU PROGRAMERS DO YOU USE.

supper_slash
supper_slash over 12 years ago

Being new to Micro-controllers, i was wanting to know what i should do to start off with as far as programers.

I am thinking PIC programers would be the best option, because of the PIC selection, but i don't know if that is a good idea.

For example, can a pic 3 Programer program ALL Pic chips, or are there limitations?  I made a mistake in buying a MSP 430 Launchpad, and although it works fine, i have a hard time figuring out what it can program, and can not program. Some chips it has listed as being able to program, i can not get it to access, and so it ended up being a wast, and at the same time, i have not yet figured out what programer Texas instrument has that will program there chips, like the pic3 programer. So, is there a couple of programmers that you all have that covers most of all of your needs? Atmel, Pic, TI, And any others? 

What do you use?

I don't haft to use pic, in fact i have never used pic, so, i am completely open to pros, and cons, and suggestions.

I just need a broad range, from 8-40 pin applications, through hole use primarily. I need to program the chip, and than place it on a board, and leave it.


Please feel free to give any ideas, or advice.  Thank-you in advance.


  • Sign in to reply
  • Cancel
  • dougw
    0 dougw over 12 years ago

    The simplest system is something like www.zbasic.net which has a free development environment and through-hole MCUs.

    The next most simple is likely arduino with a free development environment and large selection of MCU form factors and low-cost peripherals.

    I personally like the (free) PSoC Creator from Cypress Semiconductor which programs a more powerful ARM system-on-a-chip. The choice of MCUs is more limited, but the ones they have start at $4 for a through-hole card and can easily handle all the arduino-style applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago

    There are lots of microcontroller development boards that include a USB programmer.  Having a separate "MCU programmer" is not that relevant these days.  The $4 PSoC 4 boards that Douglas mentions are very attractive, except that PSoC Creator only runs on Windows.  ST has a nice series of STM Discovery boards that use the same ST-LINK programmer, which is included on the boards.  There are also a number of boards that support ARM mbed which looks like an easy way to program MCUs.

     

    I suggest choosing an MCU family you link -- the choice of programmers will be clear.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • coolbox
    0 coolbox over 12 years ago

    I think you need a "universal programmer".yes i have seen programmers which can program wide range of ICs from diffrent families like 8051,AVR and diffrent manufacturers cypreas,winbond,atmel,Nxp.Although they cover wide range but still they are not actually universal.But they are very expensive and never payback the money you invested as we always have some favorite microcontrollers and we mostly work with them.Better to select a microcontroller and then find appropriate programmers for them.you can also go for some low cost universal programmers which provide some limited selection criteria.