Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum PWM signwave with 50ns freq. Step
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 503 subscribers
  • Views 1202 views
  • Users 0 members are here
Related

PWM signwave with 50ns freq. Step

e14 Contributor
e14 Contributor over 11 years ago

Hi all,
i want to generate PWM step with 50ns. For this i have input signal.


PWM clock freq. = 24MHz.

 

 

 

if input is 3,25v  then PWM freq = 1 µs (microsec)
if input is 0,5v then PWM freq = 250ns (nanosec).

 

pls share ur ideas for doing this task.

 

Regards
Max

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1 suggested
    pls wrt n englsh bcs it wll B ezier 2 undrstnd And it really does not take much longer. When you are generating a PWM signal you need to consider two frequencies, the basic clock frequency of the generating…
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    I don't think so ! In a PWM system where one driver pulls the load high and the other pulls it low the deatime is the time when both drivers are off. It's provided by many controllers so that one device…
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    pls wrt n englsh bcs it wll B ezier 2 undrstnd

     

    And it really does not take much longer.

     

    When you are generating  a PWM signal you need to consider two frequencies, the basic clock frequency of the generating system and the pulse frequency. If you need a resolution of 1% then you will need 100 basic clock periods per pulse, so with a 24MHz clock (41.66nS period) you could have a pulse frequency of 240kHz and the pulse widths could range from 4.118uS to 41.66nS. You can' get  a 50nS step with a 24MHz clock.

     

    How are you going to generate this PWM signal  - if you are using  a timer on a micro-controller then the data sheet or user manual will usually describe how to set it up for PWM.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thank u very much for ur answer.

    I want to modulate frequency. as Input for Deadtime.

    I have i/p 3.25v for 24 Deadtime & 0.5v for 2 Deadtime.

    I have to set this in program. alöso the duty cycle have to calculate in program,

    I Need 40ns PWM Step. So PWM Clock freq. = 24MHz.

    like Deadtime values = 2 (125ns), 3(165ns), 4(205ns)....

     

    Regards

    Max

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 11 years ago in reply to e14 Contributor

    Hi Max,

     

    If you want to have a dead time, please use a microcontroller that already has a dead time generator and use that.Atmels XMEGA series have this (AWEX), and the STM32F0... devices also have this. These both run at frequencies equal or higher than 24MHz, and both have an analog to digital converter. Now the only thin you'll have to do is to read out the ADC, calculate the deadtime and write that to the peripheral.

    Here's the document which describes Atmels XMEGA options: http://www.atmel.com/images/doc8076.pdf  ,apparently you can insert 0-255 main clock cycles dead time.

    As ususal, ST's documentation and implementation is a bit more complex, as can be seen here: http://www.st.com/web/en/resource/technical/document/application_note/DM00042534.pdf,, but still you can insert dead time programmatically.



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 11 years ago in reply to e14 Contributor

    Hi Max,

     

    If you want to have a dead time, please use a microcontroller that already has a dead time generator and use that.Atmels XMEGA series have this (AWEX), and the STM32F0... devices also have this. These both run at frequencies equal or higher than 24MHz, and both have an analog to digital converter. Now the only thin you'll have to do is to read out the ADC, calculate the deadtime and write that to the peripheral.

    Here's the document which describes Atmels XMEGA options: http://www.atmel.com/images/doc8076.pdf  ,apparently you can insert 0-255 main clock cycles dead time.

    As ususal, ST's documentation and implementation is a bit more complex, as can be seen here: http://www.st.com/web/en/resource/technical/document/application_note/DM00042534.pdf,, but still you can insert dead time programmatically.