Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Measuring liquid level of a sealed container
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 497 subscribers
  • Views 3967 views
  • Users 0 members are here
Related

Measuring liquid level of a sealed container

Hasanga
Hasanga over 2 years ago

I need to measure liquid level inside a sealed container there can't be placed any sensors inside it. This is a shock absorber in a very powerful machine. So in operation the pressure and temperature will be high and flowing speed of liquid is also high . 

   1. Container is steel cylinder, height 1 meter, diameter 8 inches,          wall thickness 3 mm. it      can be tilted horizontal to 60 degrees         in vertical. But can't be            moved. It contains a nother hollow       steel cylinder.

         a. This small cylinder is same height, diameter 5 inches. And             have a orifice of 5 cm on its wall so liquid can move in and out            from this cylinder to outer cylinder freely. 

I will be measuring liquid level before operation and during trouble shooting only. What methods can be used?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz +3
    shabaz said: not realizing that just a few milli-litres causes enough vapor to be dangerous Tim Hunkin & Rex Garrod - teaspoon of gunpowder vs teaspoon of petrol: https://youtu.be/qyVHzJ40JqM?list…
  • dougw
    dougw over 2 years ago +1
    What is the liquid? How does the liquid get in and out of the cylinder? How accurately do you need to know the liquid level? Without knowing more about the system, your best bet is likely to somehow…
  • Fred27
    Fred27 over 2 years ago +1
    This sounds like a difficult problem - especially as any modification to the shock absorber could be very dangerous. Why do you want to measure the liquid level? What exactly is the problem you're trying…
Parents
  • dougw
    dougw over 2 years ago

    What is the liquid?

    How does the liquid get in and out of the cylinder? 

    How accurately do you need to know the liquid level?

    Without knowing more about the system, your best bet is likely to somehow measure the weight.

    There might be a way to use acoustic resonance, but it would require lots of experimentation. (I tried it here)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Hasanga
    Hasanga over 2 years ago in reply to dougw

    Thank you for your answer.

    This is a hydraulic liquid used in shock absorbers. It's exact name I'm not aware.

    And measuring weight is not possible as this is tightly fixed on a a big machine which moves back and forth violently when it is in operation.

    Liquid is filled in from a opening at the bottom of the cylinder and later it is sealed tightly and fixed on the machine.it can't be open again. Only on repair its open and takes long time to open and close the sealing .

    It is ok if there is a 1 to1.5  cm error in the measurement .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Hasanga
    Hasanga over 2 years ago in reply to dougw

    Thank you for your answer.

    This is a hydraulic liquid used in shock absorbers. It's exact name I'm not aware.

    And measuring weight is not possible as this is tightly fixed on a a big machine which moves back and forth violently when it is in operation.

    Liquid is filled in from a opening at the bottom of the cylinder and later it is sealed tightly and fixed on the machine.it can't be open again. Only on repair its open and takes long time to open and close the sealing .

    It is ok if there is a 1 to1.5  cm error in the measurement .