Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum MAX32666 PCM Audio subsystem keeps repeating samples
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 499 subscribers
  • Views 905 views
  • Users 0 members are here
  • max32666
  • i2s
  • audio_interface
Related

MAX32666 PCM Audio subsystem keeps repeating samples

obones
obones 11 months ago

Hello,

In an attempt at exploring the MAX32666 feature set, I'm trying to get its Audio subsystem to output a stream of bit patterns via I²S. Reading the documentation, and because the entire system is a 32bit architecture, I thought that I could use two 32 bits channels on a 64 bits frame so that no space is wasted in RAM.

Sadly, this does not to work as the lowest 8 bits are always cut out, which I reported at Analog's forums. A simple workaround is to use two 24 bits channels on a 48 bits frame so that all bits are packed without dead time in between samples.

With that out of the way I created my target samples and sent them along but could only get 900mV on the DOUT pin! As it turns out, one has to activate all four Audio pins even if you don't use them, but that's not indicated in the datasheet.

Sadly, even after that, I could not get the proper signal that I expected so I decided to create a set of samples that would allow me to clearly see what's happening on the output:

sample indexes left right
0 - 1 10000000'00000000'00000110'00000000 10000000'00000000'00001010'00000000
2 - 3 10000000'00000000'00010010'00000000 10000000'00000000'00100010'00000000
4 - 5 10000000'00000000'01000010'00000000 10000000'00000000'10000010'00000000
6 - 7 11111111'11111111'11111010'00000000 11111111'11111111'11110110'00000000
8 - 9 11111111'11111111'11101110'00000000 11111111'11111111'11011110'00000000
10 - 11 11111111'11111111'10111110'00000000 11111111'11111111'01111110'00000000
12 - 13 11111111'11111110'11111110'00000000 11111111'11111101'11111110'00000000
14 - 15 11111111'11111011'11111110'00000000 11111111'11110111'11111110'00000000
16 - 17 11111111'11101111'11111110'00000000 11111111'11011111'11111110'00000000
18 - 19 11111111'10111111'11111110'00000000 11111111'01111111'11111110'00000000
20 - 21 11111110'11111111'11111110'00000000 11111101'11111111'11111110'00000000
22 - 23 11111011'11111111'11111110'00000000 11110111'11111111'11111110'00000000
24 - 25 11000000'00000000'00000010'00000000 10000000'00000000'00000010'00000000

The basic idea is to have a marker bit be at a different place in all samples to easily identify them, while having the lowest 8 bits at zero as they will get ignored.

The code that sends all those basically does this:

Activate Audio subsystem
Turn off both TX channels
Fill transmission FIFOs (this consumes 2*4 samples)
Turn on both TX channels
While there are samples remaining, wait for space in FIFOs, place one sample for left, one for right in their respective FIFO
Now that all samples are in the FIFOs, wait for them to get empty
Turn off both TX channels

Using the "capture to file" feature of my DSO (thanks again E14, it's really a nice one), and a bit of editing in Paint.Net, I'm getting the following trace on the output pin:

image

So, the 8 queued samples are sent just fine, then an additional 4 as well, but after that, the subsystem keeps repeating samples 4 and 5 until I turn off the TX channels, for no reasons that are obvious to me.

I understand that the subsystem will repeat the last sample it has received if I'm not providing new samples fast enough, but I'm sure they are all placed in the FIFO as the while loops exit. And why repeat #4 and #5 when clearly 6 others have been given (and sent) afterwards?

In the Audio subsystem example provided in the MSDK, they are using the interrupt vector which I'll try using over the week-end to see if it helps.

In the meantime, does this situation sound familiar to any of you? Would you have any recommendation?

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones 11 months ago +3
    Well, after lots of fiddling with code, I managed to get what I want: These are timings for 26 samples sent via I2S And pushing even further, I was finally able to address all 64 LEDs with a nice…
  • shabaz
    shabaz 11 months ago +1
    I think it's probably normal that 8 bits are dropped per 32 bits and set to zero in the I2S stream, if the DAC is only a 24-bit part. I've not checked the I2S spec in a while so I could be wrong. For a…
Parents
  • shanewrn
    shanewrn 11 months ago

    it reminded me of times I’ve chased weird timing issues on microcontrollers. The way the MAX32666 repeats samples feels like one of those cases where the hardware only behaves if every setting lines up just right. I’ve run into similar FIFO and sync problems before, so it was interesting to see the same kind of troubleshooting play out and it actually gave me a couple ideas for my own projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shanewrn
    shanewrn 11 months ago

    it reminded me of times I’ve chased weird timing issues on microcontrollers. The way the MAX32666 repeats samples feels like one of those cases where the hardware only behaves if every setting lines up just right. I’ve run into similar FIFO and sync problems before, so it was interesting to see the same kind of troubleshooting play out and it actually gave me a couple ideas for my own projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • obones
    obones 11 months ago in reply to shanewrn

    Yeah, that's likely an issue here. After experimenting a bit more, even if it's not specified in the datasheet, it seems the FIFOs are implemented as ring buffers. This means that if the write pointer is no longer updated, the read pointer will eventually catch up to it and stop being updated as well, being stuck on the sample_count - buffer_size value, not the last one as the wording in the datasheet implies. That means I had to make sure there are enough "all zero" samples set in the buffers to make sure to get a final low level.