Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Companies that design PCB for honest prices?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 505 subscribers
  • Views 2319 views
  • Users 0 members are here
Related

Companies that design PCB for honest prices?

e14 Contributor
e14 Contributor over 10 years ago

Greetings,

 

I am looking for a company that is able to design a PCB, that I can send to a PCB manifacturer, starting from components.

 

My availability is not that much, I just started to look into the possibility to make the first batch of PCB, probably 50 or 100, but before I need someone that actually make the PCB design.

 

I found some that does PCB production, but not that much info about who is offering a design service; any suggestion? I would like to avoid unsafe sources; it is not nice to figure out that the design was done wrong; once you spent thousands for PCB production and components.

 

Thanks!

Luke

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1
    I would suggest designing the PCB yourself, especially since your design doesn't seem particularly complex. To find a board house that will design your board (the way you want it), mill it, and populate…
Parents
  • michaelwylie
    michaelwylie over 10 years ago

    EDIT:

    Sorry I misread the title. The service I referenced if for having a PCB fabricated.

     

    Seeed Studio's Fusion PCB service:

    Fusion PCB, customize PCB prototype | Seeedstudio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelwylie

    No problem Michael; Once I have the PCB designed I need to eventually go for a manifacturer image

     

    BTW I do not have a file to upload; I am in the phase were I have the wired prototype; so I actually need someone that design the PCB itself; so I am not sure if seedstudio is the place to go for this. I see that you need to upload a file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to e14 Contributor

    You're exactly right, they want gerber files. Gerber files define the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelwylie

    Which from a quick search, seems to require a PCB design, and this is exactly what I need help with image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to e14 Contributor

    How complicated is the design? Digital and analog?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelwylie

    Not that complex; fundamentally I have 3 sections:a microcontroller, a bluetooth to serial and a I2C chip to talk with multiple I2C devices; a voltage regulator to work with 3,3V, a battery charging chip, so I can hook up a Li-Po battery and that's all.

     

    The micro expose I2C and SPI, plus few analog in-out pins; which I would like to keep connected in case I need to expand the design. IT took me few hours to put it together with wires and breakout boards; but I would like to not have to deal with breakout boards, and make my own.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to e14 Contributor

    This sounds like an easy design. Are you going to solder the board yourself, or are you looking for a company to deliver a product with all components soldered on?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelwylie

    Most likely I won't solder the board; the components are SMC, I can solder small components but I never did IC; since their pins are too close together.

     

    I am aware that costs go up when you have the manifacturer to solder the components, but it goes long way in the overall quality of the board.

     

    One thing that I am not sure is related to the microcontroller: I use an arduino compatible board, but I assume that if I have to design the PCB, I need to include also the part that does the bootloader for the code?

    On a standard arduino compatible clone, you upload the code via usb and bootloader; not sure how would it work when you actually make a PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelwylie

    Most likely I won't solder the board; the components are SMC, I can solder small components but I never did IC; since their pins are too close together.

     

    I am aware that costs go up when you have the manifacturer to solder the components, but it goes long way in the overall quality of the board.

     

    One thing that I am not sure is related to the microcontroller: I use an arduino compatible board, but I assume that if I have to design the PCB, I need to include also the part that does the bootloader for the code?

    On a standard arduino compatible clone, you upload the code via usb and bootloader; not sure how would it work when you actually make a PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelwylie
    michaelwylie over 10 years ago in reply to e14 Contributor

    As long as it's all included in the schematic you want made into a PCB, it's just software after that. The hard part for you, it sounds, will be delivering the exact schematic you want made into a PCB. If I were doing this, I would ask for a complete schematic, and I would produce a PCB. If there was a problem in the design of the schematic, then it's not the PCB designers fault. Do you have a budget?