Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum ARM prototyping / eval board with most g i/o
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 506 subscribers
  • Views 1890 views
  • Users 0 members are here
  • embedded electronics
  • stelectronics
  • stm-32
  • mcu
  • nucleo-144
  • arm
Related

ARM prototyping / eval board with most g i/o

ghostdzog
ghostdzog over 9 years ago

Hello

i am about to start my first hardware control surface design based around an ARM M series MCU, so am presently reviewing prototyping and evaluation boards to use for my first prototype.

 

My hardware control surfaces will have lots of analogue components incorporated into them which will be connected to the general purpose ins and outs.

Some of the components will be sending signals such as faders, rotary encoders, buttons and switches and, some of the components will be used to show settings such as led's, led rings and maybe even motorised faders (but probably not to start with).

 

To start with I am likely just to use one or two of each component (one fader, one encoder etc) and will adjust my program to see if i can get the components to work with the MCU and host computer/application.

 

Once i have passed this stage, i will likely then move on to the next stage of the project, and try to set up all the components needed for the control surface (up to 25 rotary encoders, 20 buttons, and 25 led rings, and 50 single led's) to see if i can get all the components set up together and programmed to work with the board perhaps by using shift registers and strobing to get them all to work at the same time. (although i will have to look into this more at a later date).

 

However, to start with I need to choose a prototyping or evaluation board that will serve my purposes. Now, I was thinking that perhaps i should go for the prototyping board that has the most general purpose ins and outs, although, from even my basic understanding of embedded electronics, I understand that it is possible to connect even a fairly large amount of ins to a small amount of input pins with clever electronics or electronic circuit design.

 

Now, also from my very basic understanding, most the prototyping boards and eval boards are inexpensive, so the cost of my original board shouldn't be a problem and as i am designing more for personal use than mass production, the cost of the board isn't really an important deciding factor (although i do not need a board with an LCD screen or HDMI on etc).

 

What I think i need in a prototyping board, is a board that has an MCU that is powerful enough to suit my purpose. I would also like a board that has as many ins and outs which i can use to connect as many analogue components as I have. So bearing my primary objectives in mind, I would really appreciate some advice regarding which board to buy for my first and second stage prototype.

 

Also I am very new to embedded electronics but see the ST electronics Nucleo 144 boards have various ways of connecting ins to. I was wondering if someone out there could explain the difference between the various different types of ins/outs on the nucleo 144 boards, as the ST electronics site isn't great at doing this to the complete beginner.

 

Thanks for any help.

  • Sign in to reply
  • Cancel

Top Replies

  • ghostdzog
    ghostdzog over 9 years ago +1
    Thanks again for the info. I was wondering as well if you knew of any good books that explained the various components available for use when prototyping such as shift registers etc. I was also wondering…
  • ghostdzog
    ghostdzog over 9 years ago in reply to ghostdzog +1
    Hi. Just a little info. I believe the term I was looking for was Simulator. From my small knowledge, I believe that there are some simulators on the market that simulate MCU's as well as a variety of hardware…
  • ghostdzog
    ghostdzog over 9 years ago in reply to nikumar142815@gmail.com +1
    Sure. I was planning to use cloud 9 for the programming side. However, i see that there are some simulators on the market that may fit the bill for more than just the electronics / mcu simulation some…
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    You have a big learning adventure in front of you.

     

    It probably makes little difference which Nucleo board you pick at this stage. I use the Nucleo F401RE board (£9.78 from Farnell) for general purpose work. It has built in debug support and lots of IO and  a reasonable processor. There are several other boards that would work. Download the data sheet and reference manual for the processor on the board and all the documents for the board itself.

     

    In the ST world the board documents will tell you which pins are accessible on the processor and the data sheet will tell you (chapter 4) all the things they can do.

     

    The reference manual will tell you how to make them do those things.

     

    You will need to write code in C. I recommend the Keil tools (free version will do for now). The ST Cube software (free download from ST) can make basic projects for you which the Keil tools can compile ,and debug.

     

    You'll notice that I haven't quite answered your question (because each pin on the processor can do many different things)  but I hope I've told you where you can find the answers !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 9 years ago

    You have a big learning adventure in front of you.

     

    It probably makes little difference which Nucleo board you pick at this stage. I use the Nucleo F401RE board (£9.78 from Farnell) for general purpose work. It has built in debug support and lots of IO and  a reasonable processor. There are several other boards that would work. Download the data sheet and reference manual for the processor on the board and all the documents for the board itself.

     

    In the ST world the board documents will tell you which pins are accessible on the processor and the data sheet will tell you (chapter 4) all the things they can do.

     

    The reference manual will tell you how to make them do those things.

     

    You will need to write code in C. I recommend the Keil tools (free version will do for now). The ST Cube software (free download from ST) can make basic projects for you which the Keil tools can compile ,and debug.

     

    You'll notice that I haven't quite answered your question (because each pin on the processor can do many different things)  but I hope I've told you where you can find the answers !

     

    MK