Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum delay generation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 504 subscribers
  • Views 2036 views
  • Users 0 members are here
Related

delay generation

mr.rohit
mr.rohit over 9 years ago

Delay generation using timer in pic18f46k22

 

I am using timer interrupt for delay generation in pic18f

when i generate  any delay using timer that time this delay is not proper which i want,it showing some difference in time.

i want knw what is the reason of that difference ?

plz help me...

thank u..

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 9 years ago in reply to mr.rohit +4
    Well... A calculator is useful only after you fully understand, what it calculates. There is no information about age or function... First, trust the datasheet of PIC18F46K22 . Microchip tries to have…
  • koudelad
    koudelad over 9 years ago in reply to mr.rohit +4
    I am glad I could help. And welcome to element14 community To be honest, when I started with 16F PICs (13 years ago), I only had some book that didn't provide much explanation. Then I opened the datasheet…
  • koudelad
    koudelad over 9 years ago +3
    Hello, there are too many variables. The more details you add, the more we would be able to help you. Basically, I would focus on the following: 1) oscillator frequency and stability - this is crucial…
Parents
  • mr.rohit
    mr.rohit over 9 years ago

    Thanks David..

    see in CTMU there is one internal capacitor inbuild

    when we set EDGSTAT1 bit in CTMUCON register that time internal capacitor start charging using internal 5.5uA current source

    after that we have to wait some time for charging thats why we need time in microsecond,then we dissable EDGSTAT1 bit in CTMUCON register ie stop charging of internal capacitor

    so i was asked the question,becoz i want to know what happen if i use time between charging and discharging capacitor is microsecond ?

     

    Can i use the time delay in millisecond using timer interrupt for CTMU ?

     

    according to calculation when i consider time in millisecond that time voltage is increasing

    ex.

    I = 5.5uA

    T = 1ms

    C = 30pf

    V = 183.3v

     

    and  183.3 V on ADC pins for microcontroller  is not possible..

    plz share some tips for me..

    Thank you...image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mr.rohit
    mr.rohit over 9 years ago

    Thanks David..

    see in CTMU there is one internal capacitor inbuild

    when we set EDGSTAT1 bit in CTMUCON register that time internal capacitor start charging using internal 5.5uA current source

    after that we have to wait some time for charging thats why we need time in microsecond,then we dissable EDGSTAT1 bit in CTMUCON register ie stop charging of internal capacitor

    so i was asked the question,becoz i want to know what happen if i use time between charging and discharging capacitor is microsecond ?

     

    Can i use the time delay in millisecond using timer interrupt for CTMU ?

     

    according to calculation when i consider time in millisecond that time voltage is increasing

    ex.

    I = 5.5uA

    T = 1ms

    C = 30pf

    V = 183.3v

     

    and  183.3 V on ADC pins for microcontroller  is not possible..

    plz share some tips for me..

    Thank you...image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • koudelad
    koudelad over 9 years ago in reply to mr.rohit

    I think you got the CTMU wrong. There is a current source, but the voltage to be measured by ADC can't be higher than Vdd of the PIC. (It is just a regular ADC, with +Vref as Vdd or something else smaller than Vdd.) I hope no manufacturer will design a chip with such self destruction capability image

     

    Your calculation has to count with all the variables. You can set the current value of the current source, you can create variable time delay. The capacity is something you want to measure by measuring the voltage (charge) created by the current source for the time delay.

     

    To your question - with 1 ms delay, you will just measure Vdd, which is meaningless and gives you no answer about the measured capacity.

    Try to stay within Vss and Vdd boundaries otherwise your measurement makes no sense.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mr.rohit
    mr.rohit over 9 years ago in reply to koudelad

    ok thank u david..

    i think time delay in microsecond is suitable for this unit..

    i will try to maintain that boudaries...

    thank u so much...image