Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum RFID longe range detection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 503 subscribers
  • Views 498 views
  • Users 0 members are here
  • animal detection
  • rfid tag
  • rfid
Related

RFID longe range detection

octavio_mesa
octavio_mesa over 8 years ago

HI Guys.

 

I was wondering if someone knows a cheap module able to detect and identify the presence of an animal.
I need a module able to detect them in a range bigger than 10 Cm.

 

Any recommendations?

 

thank you so much.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +2
    If you can describe the situation better, it would be easier to suggest a workable solution. For example a low cost metal detector circuit could detect a small piece of steel like a dog tag from several…
  • octavio_mesa
    octavio_mesa over 8 years ago in reply to dougw +1
    Hi Douglas, Thank you for answering. I'm looking for an option similar to the RC 552 but with a bigger range of detection. RC522 RFID Module 13.56MHz | RC522-READER | I have two cats an I want that one…
Parents
  • dougw
    dougw over 8 years ago

    If you can describe the situation better, it would be easier to suggest a workable solution.

    For example a low cost metal detector circuit could detect a small piece of steel like a dog tag from several meters away, but only if there isn't other steel nearby and of course the animal would have to be wearing the dog tag.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago

    If you can describe the situation better, it would be easier to suggest a workable solution.

    For example a low cost metal detector circuit could detect a small piece of steel like a dog tag from several meters away, but only if there isn't other steel nearby and of course the animal would have to be wearing the dog tag.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • octavio_mesa
    octavio_mesa over 8 years ago in reply to dougw

    Hi Douglas,

     

    Thank you for answering.

    I'm looking for an option similar to the RC 552 but with a bigger range of detection.
    RC522 RFID Module 13.56MHz | RC522-READER |

    I have two cats an I want that one doesn't eat to food of the other, that is the reason why I need that each cat has a tag so the reader could identify what cat is and give it access to the type and quantity of food that each one eats.

    But the reader when I use this kind of tags is not able to detect all the times depends on the angle and the position that the cat has to eat.

     

    Thank you so much