Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum Build project in MPLAB, newbie question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 237 subscribers
  • Views 4490 views
  • Users 0 members are here
Related

Build project in MPLAB, newbie question

mattybee
mattybee over 13 years ago

HI,

 

This is my first foray into working with PIC microchips.  I'm trying to work with someone else's code/project notes and have tried to build the code for a

PIC16F88-I/P and getting compilation errors.  I think I've bitten off more than I can chew here image

 

Can anyone help - it may be I am doing something basic that's wrong, or perhaps the code is out of date for later versions, I just don't know.

 

Many thanks,

 

 

----------------------------------------------------------------------

Release build of project `C:\GHWT MIDI\midi.mcp' started.

Language tool versions: MPASMWIN.exe v5.49, mplink.exe v4.47, mplib.exe v4.47

Wed May 01 14:33:58 2013

----------------------------------------------------------------------

Make: The target "C:\GHWT MIDI\GHWT.o" is out of date.

Executing: "C:\Program Files\Microchip\MPASM Suite\MPASMWIN.exe" /q /p16F88 "GHWT.asm" /l"GHWT.lst" /e"GHWT.err" /o"GHWT.o"

Error[113]   C:\GHWT MIDI\GHWT.ASM 43 : Symbol not previously defined (_WRT_ENABLE_OFF)

Message[302] C:\GHWT MIDI\GHWT.ASM 71 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 72 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 76 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 79 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 82 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 88 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 91 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 99 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 124 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Message[302] C:\GHWT MIDI\GHWT.ASM 165 : Register in operand not in bank 0.  Ensure that bank bits are correct.

Halting build on first failure as requested.

----------------------------------------------------------------------

Release build of project `C:\GHWT MIDI\midi.mcp' failed.

Language tool versions: MPASMWIN.exe v5.49, mplink.exe v4.47, mplib.exe v4.47

Wed May 01 14:34:01 2013

----------------------------------------------------------------------

BUILD FAILED

 

Site links & code below:

 

http://home.cogeco.ca/~mybrainhurts/GHDrum.htm

 

http://home.cogeco.ca/~mybrainhurts/GHDRUM.txt

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 9 years ago +2
    Regarding the PIC configuration: A typical main asm file starts with these directives (copied from example asm file from MPASM folder): ;---------------------------------------------------------------…
  • keyosuke
    keyosuke over 9 years ago in reply to koudelad +2
    David, Thanks for taking the time out to debug the issue or provide information to help the initial poster and myself figure this out. I believe Matt Bayliss is probably doing what I tried to do, which…
  • koudelad
    koudelad over 9 years ago in reply to keyosuke +2
    Hello Joseph, Thank you for an explanation, now I completely understand the situation. After reading the question for the first time, I got the impression that Matt wants to continue with the development…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    The definition of  _WRT_ENABLE_OFF is not found in yout project.

    You will have to check if you have included all the libraries and header files for your project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mattybee
    mattybee over 13 years ago in reply to e14 Contributor

    Thanks for your reply, I think I've got it, as you correctly state, there is no definition for WRT_ENABLE_OFF in the header, I found a WRT_OFF which seems to have a similar function and changing the code fixes this.

     

    I still get the other errors and although in the code there are references to 16F88 perhaps it's for an older version.  Unfortunately although the project notes are pretty complete there is no apparent way to contact the author.

     

    Message[302] C:\GHWT MIDI\GHWT.ASM 72 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 73 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 77 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 80 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 83 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 89 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 92 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 100 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 125 : Register in operand not in bank 0.  Ensure that bank bits are correct.

    Message[302] C:\GHWT MIDI\GHWT.ASM 166 : Register in operand not in bank 0.  Ensure that bank bits are correct.

     

    As a newcomer to PIC this is beyond me to fix I think.  Oh well.

     

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mattybee

    Hello Matt,

     

    I remember having teh similar problem earlier.

    I solved it by setting or clearing(I dont remember now) R0 in the status register(STATUS).

    This setting and clearing was done in the code, there was also the possibility to set this bit in IDE.

     

    Check it out.......

     

    Write back if you did not find how to set/clear the bit 0 in Status register.

     

    srkjfone

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mattybee

    Hello Matt,

     

    I remember having teh similar problem earlier.

    I solved it by setting or clearing(I dont remember now) R0 in the status register(STATUS).

    This setting and clearing was done in the code, there was also the possibility to set this bit in IDE.

     

    Check it out.......

     

    Write back if you did not find how to set/clear the bit 0 in Status register.

     

    srkjfone