Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum 8 bit PIC with RTC chip.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 232 subscribers
  • Views 3434 views
  • Users 0 members are here
Related

8 bit PIC with RTC chip.

asanyi
asanyi over 3 years ago

Hi, my circuit is composed from a PIC16F15345 microcontroller and a MCP79411 RTC chip, connected with i2c, it has an own 32.768 crystal. The 16F15345 also drives deprez meters and LEDs with PWM signals. While the power of the main circuit is switched off, the RTC runs correctly (precise timing) from its backup 3V battery. But activating the power of the PIC and the PWM driving, the RTC has lost its correct operation, delaying 30 minutes per 12 hour! Any idea to fix is accepted...

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago in reply to asanyi +2
    You will have far more success if you learn to plan and draw schematics. Even if freehand in your notebook they can be copied. What is a "deprez solenoids" MK
  • asanyi
    asanyi over 3 years ago in reply to ggabe +2
    Main power at normal operation, 5V: supplied the PIC VDD pin, supplied the MCP79411 RTC on pin8 VDD, supplied the anods of the LEDs. The deprez coil are drived from PWM pins of the PIC VIA NPN transistors…
  • michaelkellett
    michaelkellett over 3 years ago +1
    You need to show us the circuit diagram and ideally some pictures of the hardware. The kind of problem you describe is often caused by bad layout, inadequate power supply decoupling or ciruit errors…
Parents
  • misaz
    misaz over 3 years ago

    Do your board follow general recommendations for crystals like following?

    • No component under crystal, only ground plane
    • Groud plane around crystal from all sides on the same layer
    • Traces to chip as short as possible and preferably both the same size
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • asanyi
    asanyi over 3 years ago in reply to misaz

    Thanks, the recommendations are clear, but to easy to realize on a prototype board, check the attached photo. So it is not the best one, additionally the RTC chip is soldered into a SOIC/DIP PCB. But similar layout worked well in other boards. Only if a PWM is running, I have the problem. Can be the root cause the interference between the frequency of the RTC osc (32.768 Hz) and the used PWM period=32msec (31.25kHz)? May I try with totally different PWM period?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago in reply to asanyi

    Is your PWM output on pin number 3?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 3 years ago in reply to asanyi

    Is your PWM output on pin number 3?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • asanyi
    asanyi over 3 years ago in reply to misaz

    The PWM signals are generated by the PIC, as all together 4 PWMs I need: meter for hours, meter for minutes, LED backlight for hour meter, LED backlight for minutes meter (these are bright regulated depends on the lighting of the environment), I use the PWM3, PWM4, PWM5, PWM6 capability of the PIC16F15345, pin7, pin6, pin5, pin8. All PWM channels are running from TMR2, with same base period, but separatelly programmable duty%. This part works well, I have wondered that this small PIC has 6 PWM outputs.