Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum PIC10F microcontroller output pin tolerance to overriding voltages
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 232 subscribers
  • Views 2125 views
  • Users 0 members are here
Related

PIC10F microcontroller output pin tolerance to overriding voltages

davebullockmbe
davebullockmbe over 2 years ago

I am using PIC10F microcontrollers in a wireless project that has evolved into needing to use an 'in circuit' programmable radio IC.

The problem is that the GP2 pin of the PIC would be connected to the DATA input (and programming) pin3 of the radio IC.
The whole circuit is running off 3v7 lipo battery.
My question is will the PIC GP2 output be destroyed when programming the radio IC. ?

Thanks in anticipation....

Daveimage

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago in reply to davebullockmbe +2
    You can set GP2 as an input to prevent it from loading the radio pin during programming: From the Microchip data sheet. 5.2 TRIS Registers The Output Driver Control register is loaded with the contents…
  • JWx
    0 JWx over 2 years ago

    maybe some OR gate could be placed between if external programming is needed? Or even removable jumper - even if GP2 will not be destroyed by forcing it into opposite state, it could interfere with programming signal...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 2 years ago

    Could you use a Schottky diode in series to protect the PIC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • davebullockmbe
    0 davebullockmbe over 2 years ago in reply to dougw

    HI thanks for your considered replies. I had thought about a jumper but board space is too tight.  Maybe I can make room for a 0402 schottky diode though. I was hoping I would get away without reworking the board but you have confirmed my doubts. Thanks Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 2 years ago in reply to davebullockmbe

    You might also need a pull down resistor unless you can just short out D2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 2 years ago in reply to davebullockmbe

    Actually, you could replace R6 with a diode and D2 with a resistor. Then you would just need a jumper to the data pin (and a cut to the original path).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 2 years ago

    If you could hold the processor in reset, GP2 would be tri-stated...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • davebullockmbe
    0 davebullockmbe over 2 years ago in reply to scottiebabe

    Yes the problem with adding a diode in series with the data line is as you say the data pin of the radio chip will float and so need a resistor to pull it down. Unlike Microchip datasheets I cannot find any information about the internal structure of these radio IC's ie. whether they have internal pull-ups/downs. I have just about run out of board space and am struggling to add even one more component.
    However putting the PIC10F202 into reset would be a great idea but doesn't this need extra PIC code to force the o/p pins into tristate. I don't think toggling MCLR does this on it's own?
    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 2 years ago in reply to davebullockmbe

    You can set GP2 as an input to prevent it from loading the radio pin during programming:

    From the Microchip data sheet.

    5.2 TRIS Registers
    The Output Driver Control register is loaded with the
    contents of the W register by executing the TRIS f
    instruction. A ‘1’ from a TRIS register bit puts the corresponding
    output driver in a High-impedance mode. A
    ‘0’ puts the contents of the output data latch on the
    selected pins, enabling the output buffer. The exceptions
    are GP3, which is input only and the GP2/T0CKI/
    COUT/FOSC4 pin, which may be controlled by various
    registers. See Table 5-1

    MK