Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Pic Microcontrollers Forum FizzBuzz in PIC16f877A driving me crazy..
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 234 subscribers
  • Views 343 views
  • Users 0 members are here
Related

FizzBuzz in PIC16f877A driving me crazy..

madthescientist
madthescientist 2 months ago

I am trying to create a firmware for Pic16f877A, using mplab 6.15 on gnu/linux and  pickit 3.

After finding out code examples in C language i could try and test parts to build a working piece of source code for it. However, i am finding myself at odds whenever i do wish to get actual work done.

I do wish to drive some leds on an off in sequences, sometimes turning on one, off other several times and holding them off some minutes to do it back. I could accomplish part of it using something called "fizz buzz" example and reading ticks from Timer 1's prescaler. My C and PIC knowledge is not yet the best.

The major problem i am struggling with is that, i can get 2 leds toggling one after the other, but if i try to get that within a FOR cycle, it either never stops if i do not add any code at FOR's end, or if i add code, it inmediatly jumps to it avoiding to toggle the leds altogether. If i code them off after for() they stay off, if i code them on after for, they stay offf.

The source code i am in trouble with is this one:

void MainProgramme(void)
{
/*Essential Variables Are Declared Here*/
Led3 = 0; //Seems It Has To Be Turned Explicitly Off Before Anything...

unsigned int tick = 0; //A Common Variable For Measuring Timer0 Ticks
unsigned int activations = 0; //This Is For Counting Movements.
unsigned int times = 0; //This Is For Counting SubFunction Executions.
unsigned int blinks = 0;// This Is For Programme Led Blink Timer 0 Overflow Counting.
unsigned int counter = 1;


/*The Function Actually Starts Here*/

while(Button1 == 0) //Checks If Button1 Is Depressed Aiming Towards Turning Off The Machine
{
while(Run == 0) //Checks If Run Button Is Depressed Toggling Between Work Or Pause
{
/******************************************************************************************************/
/*Main Led Stays Blinking At Around 2hz While The Procedure Takes Place If Not Paused*/

tick++;

// Check if Timer0 has overflowed
if(TMR0IF == 1)
{
TMR0IF = 0; // Reset the flag immediately
blinks++;

// 7 overflows ~ 458ms (close to 0.5s for 1Hz toggle)
if(blinks >= 266) {
MainLed = ~MainLed; // Toggle LED on RB0
blinks = 0; // Reset counter

}



/**********************************************************************************************************/
if(Led7 == 0)
{
//--------------------------------------------------------------
while(Switch2 == 0)
{

Blink2 = 0;
Blink1 = 0;
Led3 = 0;

// Timer 0 For Programme Led Blinking. IT WORKS, AVOID BREAKING.
// Check if Timer0 has overflowed
if(TMR0IF == 1)
{
TMR0IF = 0; // Reset the flag immediately
blinks++;

// 7 overflows ~ 458ms (close to 0.5s for 1Hz toggle)
if(blinks >= 266) {
MainLed = ~MainLed; // Toggle LED on RB0
blinks = 0; // Reset counter

}
} Led6 = 1;
} Led6 = 0;
} // Main Programme Led Blink Ends Here. AVOID TOUCHING THIS PART, IT WORKS.
//------------------------------------------------------------------------
if(Led7 == 1)
{
while(Switch1 == 0)
{

Blink2 = 0;
Blink1 = 0;
Led3 = 0;

// Timer 0 For Programme Led Blinking
// Check if Timer0 has overflowed
if(TMR0IF == 1)
{
TMR0IF = 0; // Reset the flag immediately
blinks++;

// 7 overflows ~ 458ms (close to 0.5s for 1Hz toggle)
if(blinks >= 266) {
MainLed = ~MainLed; // Toggle LED on RB0
blinks = 0; // Reset counter

}
}
Led6 = 1;
} Led6 = 0;
} // Main Programme Led Blink Ends Here. AVOID TOUCHING THIS PART, IT WORKS.
//------------------------------------------------------------------------------------------------




//Timer 1 For Blink Led Timings
while(Switch1 == 1 || Switch2 == 1)
{


/************************************************************************/
/*Programme Led Seems To Be Blinked Locally*/
// Check if Timer0 has overflowed
if(TMR0IF == 1)
{
TMR0IF = 0; // Reset the flag immediately
blinks++;

// 7 overflows ~ 458ms (close to 0.5s for 1Hz toggle)
if(blinks >= 198) {
MainLed = ~MainLed; // Toggle LED on RB0
blinks = 0; // Reset counter

}
}
/*************************************************************************/
//This Is Timer 1 Setting leds Timings.Timer 0 Sets Programme Led Blinking
if (PIR1bits.TMR1IF) { // Check if Timer1 overflowed
PIR1bits.TMR1IF = 0; // Clear flag
TMR1H = 0x00; // Reload timer
TMR1L = 0x00;


counter++;
if (counter > 200) counter = 1; // Loop 1 to 100
}



if((MainStrenghtRedLed == 0) && (MainStrenghtGreenLed == 1))
{
for(times = 10; times >= 0; times --)
{

if (counter % 3 == 0)
{
times = times + 1;
Blink1 = 0;
Blink2 = 1;
} else if (counter % 5 == 0)
{
Blink1 = 1;
Blink2 = 0;
} else if (counter % 7 == 0)
{
Blink1 = 0;
Blink2 = 1;
}

else if (counter % 9 == 0)
{
Blink1 = 1;
Blink2 = 0;
}

else if (counter % 11 == 0)
{
Blink1 = 0;
Blink2 = 1;
}

else if (counter % 13 == 0)
{
Blink1 = 1;
Blink2 = 0;
}

else if (counter % 15 == 0)
{
Blink1 = 0;
Blink2 = 1;
activations--;
}


} //It's suposed to perform this FizzBuzz routine a couple of times and stop, then again for some times.
Problem is: it never stops. If i do add any code after the For() it actually jumps to it.
}
}Led6 = 1; //End Of While



/*******************************************************/
}

/*******************************************************/
}
}__delay_ms(100);
PowerOff();
}

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J 2 months ago +1
    Do you have a routine that sets up the input/output pins and the timers?
Parents
  • vmate
    0 vmate 2 months ago

    I don't quite fully understand what you did so far and what the goal would be, but I can see several problems:

    The for loop you made is an infinite loop, because 'times' is unsigned, aka. it can never be lower than 0, and the condition for the for loop to finish is 'times' being lower than 0.

    Also, the 'if (counter % 3 == 0)' part increments 'times', and the for loop decrements it, so they are actively fighting one another. You might've intended for that to happen, but this is not generally a good idea to do: the rule of thumb is to use a for loop if you already know how many times you want the loop to run, or use a while loop if you don't.

    Another problematic part is the speed of execution. You're checking the counter's value in the for loop in multiple places, but that loop will execute many thousands of times faster than the counter's increment speed.

    If I were you, I'd probably start from scratch, and ignore the hardware timer for now. Have a big while(1) loop with a __delay_ms(10); at the end, and just increment your own counter somewhere. Getting an Arduino, and going through the Arduino IDE's examples(like 'Blink without delay()') to learn the logic and program flow for such a microcontroller would probably be the ideal path, as the learning curve is much gentler there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vmate
    0 vmate 2 months ago

    I don't quite fully understand what you did so far and what the goal would be, but I can see several problems:

    The for loop you made is an infinite loop, because 'times' is unsigned, aka. it can never be lower than 0, and the condition for the for loop to finish is 'times' being lower than 0.

    Also, the 'if (counter % 3 == 0)' part increments 'times', and the for loop decrements it, so they are actively fighting one another. You might've intended for that to happen, but this is not generally a good idea to do: the rule of thumb is to use a for loop if you already know how many times you want the loop to run, or use a while loop if you don't.

    Another problematic part is the speed of execution. You're checking the counter's value in the for loop in multiple places, but that loop will execute many thousands of times faster than the counter's increment speed.

    If I were you, I'd probably start from scratch, and ignore the hardware timer for now. Have a big while(1) loop with a __delay_ms(10); at the end, and just increment your own counter somewhere. Getting an Arduino, and going through the Arduino IDE's examples(like 'Blink without delay()') to learn the logic and program flow for such a microcontroller would probably be the ideal path, as the learning curve is much gentler there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • madthescientist
    0 madthescientist 2 months ago in reply to vmate

    I named it unsigned since most examples i found in the web uses unsigned, i did not know that it prevents it to reach zero.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett 2 months ago in reply to madthescientist

    An unsigned variable can reach zero, but it can't be negative.

    Change

    for(times = 10; times >= 0; times --)

    to

    for(times = 10; times > 0; times --)

    or better to

    for(times = 0u; times < 10u; times++)

    (The u tells the C compiler that the 10 (and the 0) are unsigned - arguably pedantic and it will work without in this case)

    (and when you have  a free choice make your 'for' loops increment because it's much more common and will help you avoid the occasional silly error, and you never get caught by the >=0 trap)

    I find your code almost impossible to follow because there is no indentation - is this because you didn't use any or because E14 lost it ?

    It would be good if you could repost it with indentation if you can:

    image

    (I did this in Notepad++ set for C language)

    The indentation style is based on https://barrgroup.com/sites/default/files/barr_c_coding_standard_2018.pdf

    I'll take another look then and see if I can work out what is happening.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave 2 months ago in reply to michaelkellett
    michaelkellett said:
    is this because you didn't use any or because E14 lost it ?

    Probably because the Code widget defaults to 'Text'

    image

    and needs to be set to 'C'