Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Polls Breakout board for a BGA chip
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 2 Jun 2019 2:34 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 3509 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

Breakout board for a BGA chip

printf(F("Hello World!));

 

I am planning a breakout board for an BGA chip and have so many decisions, that I would like to get some input from the community.

 

The BGA is a 5mm x 5mm 24-ball BGA (pin A1 is missing). The device is the VLSI VS23S040 Composite Video/RGB/VGA + Memory controller.

To make the part usable I would add the crystal and bypass capacitor to the breakout board.

 

Some options that make sense to me are:

  • 2.54mm (0.1") pitch, pins on 4 sides: 18mm x 18mm size, easy to handle and solder, not so easy to test. Not testable with horizontal pogo pins.
  • 2.54mm (0.1") pitch, pins only on 2 opposite sides: 32mm x 10mm size, to be usable on a prototype board, the pins could only be on 2 sides. This would make the board unnecessary big, but more versatile.
  • 2mm (80mil) pitch, pins on 4 sides: 14mm x 14mm size, would give the smallest area footprint and be still easy to solder. Not testable with horizontal pogo pins.
  • 1.27mm (50mil) pitch, pins on 4 sides: 9mm x 9mm size, BGA only without crystal. Smallest size ever.
  • 1.27mm pitch, pins on 2 sides: 16mm x 8mm size, very small with crystal and testable with pogo pins.

 

Ideas for any other configurations. Please tell me in the comments

 

Thanks for having an opinion.

 

- W.

 

PS: I was hoping the image are comparable scale, but they are not.

  • composite
  • vs23s040
  • video
  • bga
  • breakout
  • NTSC
  • vga
  • pal
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to Fred27 +3
    Good points. The idea is to make an interesting chip (at least I think it is) more accessible for a range of people who tent to build their own systems. Yes the plan is to have thoseboards up for sale…
  • Fred27
    Fred27 over 7 years ago +3
    I've gone for 0.1" pitch in two rows. Making it easy to prototype is a higher priority than making it small. I assume your main market will be someone who wants to add a VGA display to a microcontroller…
  • dougw
    dougw over 7 years ago +3
    I like this - it is a good idea. (Because I am not set up to handle BGAs yet) As someone who might buy such a product, I prefer the last option if it comes with the crystal and chip pre-assembled, because…
  • clem57
    clem57 over 7 years ago

    This is what caught my eye:

    to be usable on a prototype board, the pins could only be on 2 sides.

    Anything breadboard dimensions allow experimentation without a soldering iron.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago

    That's a really interesting part. Although it's quite small the BGA is 1mm pitch which is reasonably prototype assembly friendly.

     

    I'd go for the bigger board with 2.54mm pitch pins and a footprint for crystals to support PAL or NTSC.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to wolfgangfriedrich

    I am mostly interested in NTSC composite output if that helps.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to dougw

    Thanks for confirming my other thoughts. If it is not breadboard compatible, make it as small as possible but still functional.

     

    On a side note, the crystal footprint would restrict this board to be VGA only. For the PAL/NTSC composite video I would need very special frequencies of 4.433618/3.579545 MHz. Lo and behold, they are only available in variants of the good old HC49 can. Custom crystals are probably out of reach for expected low quantities.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago

    I like this - it is a good idea. (Because I am not set up to handle BGAs yet)

    As someone who might buy such a product, I prefer the last option if it comes with the crystal and chip pre-assembled, because it can be inefficient to buy a specific crystal for a specific footprint in single quantity.

    I would not run something like this from a breadboard, I would always solder it to a custom MCU PCB, so smaller is better.

    With 0.05" pitch I wouldn't be running traces between pins, but it would be nice to be able to run traces between the 2 rows of pins instead of creating a large no-fly zone where the module sits.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to Fred27

    That would be plan B. A so-called Shieldwing or Wingshield (you heard it here first), a full module with VGA connector, all support circuit and 2 sets of connector to be either an Arduino shield or a Feather wing. This would be much easier to prototype with. I might shelf the whole breakout board idea.

    Yes, the PCB cost would be minimal. the biggest factor is getting everything ready to be sell-able is a huge time effort. And doing it twice for almost the same thing might not be worth it.

    Thanks for having an opinion.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago

    I've gone for 0.1" pitch in two rows. Making it easy to prototype is a higher priority than making it small. I assume your main market will be someone who wants to add a VGA display to a microcontroller. I would have thought they might use your board to test their idea out. I suspect that for this design, full through holes would be better than castellated ones. A footprint for a VGA connector would be good on this sort of board too. That way it can be more easily prototyped.

     

    If they're worried about size then they might then either spin up their own board or use one of you smaller SMT modules - preferably with the required passives like the last one.

     

    As getting the PCBs made is unlikely to be the costly bit it might be worth trying both these options.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to Fred27

    Good points.

    The idea is to make an interesting chip (at least I think it is) more accessible for a range of people who tent to build their own systems. Yes the plan is to have thoseboards up for sale at some point. Testing will be mostly important for me to know that I send working products. I like the idea of horizontal pogo pins using the spring force to hold the UUT in place, which only works for the 2-row versions. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago

    The "best" option really depends on how you intend to use it. It's not something a poll can help you decide - unless we're your target sales market. For instance, how does being testable with horizontal logo pins help? Will you be making and testing a lot of these?