Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Polls Breakout board for a BGA chip
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 2 Jun 2019 2:34 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 3510 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

Breakout board for a BGA chip

printf(F("Hello World!));

 

I am planning a breakout board for an BGA chip and have so many decisions, that I would like to get some input from the community.

 

The BGA is a 5mm x 5mm 24-ball BGA (pin A1 is missing). The device is the VLSI VS23S040 Composite Video/RGB/VGA + Memory controller.

To make the part usable I would add the crystal and bypass capacitor to the breakout board.

 

Some options that make sense to me are:

  • 2.54mm (0.1") pitch, pins on 4 sides: 18mm x 18mm size, easy to handle and solder, not so easy to test. Not testable with horizontal pogo pins.
  • 2.54mm (0.1") pitch, pins only on 2 opposite sides: 32mm x 10mm size, to be usable on a prototype board, the pins could only be on 2 sides. This would make the board unnecessary big, but more versatile.
  • 2mm (80mil) pitch, pins on 4 sides: 14mm x 14mm size, would give the smallest area footprint and be still easy to solder. Not testable with horizontal pogo pins.
  • 1.27mm (50mil) pitch, pins on 4 sides: 9mm x 9mm size, BGA only without crystal. Smallest size ever.
  • 1.27mm pitch, pins on 2 sides: 16mm x 8mm size, very small with crystal and testable with pogo pins.

 

Ideas for any other configurations. Please tell me in the comments

 

Thanks for having an opinion.

 

- W.

 

PS: I was hoping the image are comparable scale, but they are not.

  • composite
  • vs23s040
  • video
  • bga
  • breakout
  • NTSC
  • vga
  • pal
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to Fred27 +3
    Good points. The idea is to make an interesting chip (at least I think it is) more accessible for a range of people who tent to build their own systems. Yes the plan is to have thoseboards up for sale…
  • Fred27
    Fred27 over 7 years ago +3
    I've gone for 0.1" pitch in two rows. Making it easy to prototype is a higher priority than making it small. I assume your main market will be someone who wants to add a VGA display to a microcontroller…
  • dougw
    dougw over 7 years ago +3
    I like this - it is a good idea. (Because I am not set up to handle BGAs yet) As someone who might buy such a product, I prefer the last option if it comes with the crystal and chip pre-assembled, because…
Parents
  • dougw
    dougw over 7 years ago

    I like this - it is a good idea. (Because I am not set up to handle BGAs yet)

    As someone who might buy such a product, I prefer the last option if it comes with the crystal and chip pre-assembled, because it can be inefficient to buy a specific crystal for a specific footprint in single quantity.

    I would not run something like this from a breadboard, I would always solder it to a custom MCU PCB, so smaller is better.

    With 0.05" pitch I wouldn't be running traces between pins, but it would be nice to be able to run traces between the 2 rows of pins instead of creating a large no-fly zone where the module sits.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 7 years ago in reply to dougw

    Thanks for confirming my other thoughts. If it is not breadboard compatible, make it as small as possible but still functional.

     

    On a side note, the crystal footprint would restrict this board to be VGA only. For the PAL/NTSC composite video I would need very special frequencies of 4.433618/3.579545 MHz. Lo and behold, they are only available in variants of the good old HC49 can. Custom crystals are probably out of reach for expected low quantities.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to wolfgangfriedrich

    I am mostly interested in NTSC composite output if that helps.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 7 years ago in reply to wolfgangfriedrich

    I am mostly interested in NTSC composite output if that helps.

    • Cancel
    • Vote Up +3 Vote Down