Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help selecting an amplifier IC
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 340 subscribers
  • Views 5050 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help selecting an amplifier IC

jimmy5893
jimmy5893 over 5 years ago

I am working on a project with 2 other classmates of mine. We are using the analog devices ADAU1701 DSP to process audio from a device using a 3.5 mm jack. We are not using the development board, so we need to find an amplifier IC. I am looking for an IC that can provide enough power for most headphones. I have seen all sorts of numbers floating around so I am confused about what would be appropriate. The supply voltage to the IC is 8V DC max. It also can't be too hard to solder on to a PCB. I could use some help.

 

I initially was looking at TI for chips and I noticed that a lot of their "hi-fi" chips only output 0.1w or less at 16 or 32 ohms. This confused me because I have a dedicated amp (liquid spark) for my planar magnetic headphones which is a Fostex T60rp (modded), and it outputs 1.3W at 50 ohms. Some other forums said that 1 to 2 milliwatts are enough because most headphones have a sensitivity of 90-115 dB/mW. 

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +4
    Hi Jimmy, I recently ordered in a couple of these and found them to work pretty good: https://www.ebay.com/itm/LM386-MINI-Mono-Amplifier-Module-3V-12V-US-Seller-Fast-Shipping/111745624072?ssPageName=STRK…
  • shabaz
    shabaz over 5 years ago +4
    Hi Jimmy, A few milliwatts or low tens of milliwatts is sufficient for typical headphones or earphones. Mobile phones only output a few tens of mW to the headphone socket, and that's good enough for typical…
  • jimmy5893
    jimmy5893 over 5 years ago in reply to jw0752 +2
    Thank you, I will look into it. From the data sheet of the LM386, it can provide 325mW at 6V. So is an amplifier chip that has between 100mW and 500mW adequate for most headphones? One other thing is that…
  • shabaz
    shabaz over 5 years ago in reply to jimmy5893

    This conversation is getting a bit audiophile, meaning the conversation doesn't make any more sense technically to me.

    I've yet to hear any normal headphones that don't function with a LM386 or a mobile phone. I have listened to $200+ head- and ear-phones and they sound fine with a typical mobile phone.

    If the THD is too high, you'll have to search for a design which has lower THD. It won't make the project very hi-fi anyway, because if you were interested in that, you would not be using the in-built analog output from the DSP.

     

    Sounds like the project just changed from a DSP amplifier to an audiophile headphone amplifier project.. in which case there are online schematics of such amplifiers you could examine (there are audiophile websites with these schematics).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jimmy5893
    jimmy5893 over 5 years ago in reply to shabaz

    Sorry if I am being scrambled in my thoughts and reasoning. You do have a point that this won't be the highest fidelity. It is still a DSP project, but if I can find an IC that will be good enough for headphones with 300 ohms like the popular HD600 from Sennheiser then it will be suitable. I just want enough power to make those have enough volume and decent enough sound quality. I'm not saying the LM386 can't because I don't know, but if you're comparing it to a mobile phone then I would be concerned. If it can outperform a mobile phone and drive higher impedance headphones decently, then I can use it. I initially said I might not use it is because it is mono. My friend is making the PCB and soldering the components so he said he would prefer 2 channel/stereo IC. The LM4880 or LM4881 is something we are looking into because it is stereo, but we are still looking.

    Edit: My friend told me that the DSP itself is .9Vrms or 2.5V peak to peak. So, I don't think I need as much power as I was expecting, right? He was saying that this level can drive earbuds and low impedance headphones, but we still want to add another amplifier to drive higher impedance headphones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • aswinvenu
    aswinvenu over 5 years ago

    Hi Jimmy,

     

       Why don't you build a stereo amplifier using two LM386 on a prototyping board and test it with your headphone. If you are satisfied with the result then use it for the project.

    It won't take much time to build one from scratch.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to jimmy5893

    Hi Jimmy,

    Here is a place you can buy a small stereo amplifier for $5 and they throw in two speakers to boot. These are the type of desk computer speaker I was referring to.

     

    https://www.parts-express.com/sound-force-505-powered-computer-speaker-pair--319-122?gclid=CjwKCAjwtNf6BRAwEiwAkt6UQotU-_QwkVShUNMpFSfAN9QkOqIiNw_-40LGPmPPDoDPwX8FuWQ1qBoC45UQAvD_BwE

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to jimmy5893

    jimmy5893  wrote:

     

    good enough for headphones with 300 ohms

     

    That's unrealistic. You're asking for some high power stereo chip to drive up to 3W for one set of headphones because a mobile phone type amplifier isn't good enough, and now to drive high voltage high impedance too, with THD requirement better than typical single-chip headphone amplifiers. I think you may have to design a custom circuit, or just use normal headphones.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hugohu
    hugohu over 5 years ago

    It can't be too hard to solder on a PCB

     

    I'd recommend one of the chips from Maxim Integrated, MAX9716/9717, they can drive a mono speaker 1.4W at 4 ohms and 1W at 8 ohms.

     

    They also feature headphone sensing.

     

    It also comes in a 3x3mm uMax package.

     

    Only managed to solder one on a breakout board.

     

    The input for it is 2V-5.5V I think, which isn't that bad.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jimmy5893
    jimmy5893 over 5 years ago in reply to jw0752

    Is there a decent amplifier chip you would recommend?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jimmy5893
    jimmy5893 over 5 years ago in reply to shabaz

    3W is definitely too high of an expectation. I read that that the max power for the HD600 is less than .5W so that would be the maximum target at this point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jimmy5893
    jimmy5893 over 5 years ago in reply to aswinvenu

    I heard that the LM386 is okay enough, but my friend wants a stereo IC so he doesn't have to solder two chips. Is there another option that comes to mind?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jimmy5893
    jimmy5893 over 5 years ago in reply to hugohu

    I haven't heard of maxim integrated so this is good, as I can look at another company now. Is there a stereo chip you can recommend?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>