Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need some help choosing a 0.96" OLED and a connector
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 339 subscribers
  • Views 5860 views
  • Users 0 members are here
  • oled
  • ssd1306
  • ffc_cable
  • display
  • ffc/fpc_connector
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need some help choosing a 0.96" OLED and a connector

starfox5194
starfox5194 over 5 years ago

image

I am trying to fit this 0.96" SPI OLED SSD1306 screen into my dash cluster. Although the screen fits, the controller board must be relocated.

I want to use SPI, not I2C for the draw speed.

image

Problem is, I damaged the screen when I used a heat gun to de-solder the screen from the control-board. Screen still kind of works, but I would like to re-do this with less soldering down the road.

 

This SPI display does not come with a controller board, and the connection is a 30-pin 0.7mm pitch. 0.7mm is non-standard, so I can't find a connector to make a solder-free extension.

https://www.buydisplay.com/datasheet-128x64-oled-module-spi-0-96-inch-graphic-displays-white-on-black

 

This I2C display uses a 0.5 mm pitch. But I don't know if there is a controller board that I can connect this to that is cheap and affordable.

https://www.buydisplay.com/128x64-oled-i2c-0-96-display-white-color-connector-fpc-ssd1306

 

Does anyone have any suggestions for me? I really need to keep the 0.96" dimension, I just need a way to relocate the breakout board with ease!

 

Thanks,
Alex

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 5 years ago +2
    Redesigning the PCB might be the easiest. Your other option would be to design a longer flex PCB to replace the existing one. That would be interesting to do, but likely to be more expensive - and quite…
  • Fred27
    Fred27 over 5 years ago +1
    I seem to be having permission problems seeing the photos you've attached.
  • starfox5194
    starfox5194 over 5 years ago in reply to shabaz +1
    Sorry the photos were not working. I tried uploading them to imgur this time. https://imgur.com/a/peHIm8c The controller board I am referring to is the OLED controller board, not the microcontroller board…
Parents
  • dougw
    dougw over 5 years ago

    I you have damaged the display, maybe a new display with easier wiring is an option:

     

    .96" TFT color SPI.96" TFT color SPI

     

    .96" OLED.96" OLED

     

    .96" color OLED.96" color OLED

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to dougw

    Good suggestion , the middle option looks best.

     

    @Fred27 , the flex board on this type of display is usually an integral part of the display and often carries the interface chip - it's not replaceable.

     

    @starfox5194 , these flexible PCB display interfaces are very difficult to manage unless you have a good production process sorted out. I've seen

    prototype workshops with a lot of pcb experience come to grief with them. So much so that I gave up specifying them a long time ago. Doug's suggestion

    is your best bet.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • starfox5194
    starfox5194 over 5 years ago in reply to michaelkellett

    Thanks for the ideas, all.

     

    i am still thinking my best option here is to redesign the oled “flex board” to properly fit in the space I require. It is a pretty simple pcb, and moving around a few traces shouldn’t be too hard. This will be a good learning experience.

     

    re-soldering the ffc is also not too difficult if it is just to connect to a properly designed pcb. Also, the oled displays are a couple of dollars, so it’s fine if a few break in the process.


    i think switching to an entirely different display at this point would not be a good idea, unfortunately all of the displays I saw Doug link to would probably still have the same issue I am currently experiencing.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • starfox5194
    starfox5194 over 5 years ago in reply to michaelkellett

    Thanks for the ideas, all.

     

    i am still thinking my best option here is to redesign the oled “flex board” to properly fit in the space I require. It is a pretty simple pcb, and moving around a few traces shouldn’t be too hard. This will be a good learning experience.

     

    re-soldering the ffc is also not too difficult if it is just to connect to a properly designed pcb. Also, the oled displays are a couple of dollars, so it’s fine if a few break in the process.


    i think switching to an entirely different display at this point would not be a good idea, unfortunately all of the displays I saw Doug link to would probably still have the same issue I am currently experiencing.