Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using transformer secondary windings
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 302 subscribers
  • Views 2088 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using transformer secondary windings

colporteur
colporteur over 4 years ago

image

Can I use both secondary windings to power separate loads?

 

I have a need for two 4.5VAC power supplies.

I have a transformer that is 9VAC with a center tap. I would like to connect one load to one 4.5VAC O/P and the other load to the other 4.5VAC. I'm assuming I can do this, provided I don't exceed the max current rating. It has been a long time since I have dabbled this low in analogue. I was looking for some reassurance or refresher.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago in reply to Jan Cumps +3
    Thanks JC for the reply. The AC loads are two small model railroad buildings that require 4.5VAC. It looks like they have some internal electronics to generate power for the few LEDS scatter around. It…
  • gdstew
    gdstew over 4 years ago +1
    As far as I can remember you can use a half wave rectifier on both output taps and the share the center tap as ground there is no problem with the circuits connecting to each other. Using half wave rectification…
  • colporteur
    colporteur over 4 years ago in reply to gdstew +1
    Only need the AC. I have no need for the rectifier stuff.
Parents
  • colporteur
    colporteur over 4 years ago

    Worked like a charm the very first time. Thanks for for your input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 4 years ago

    Worked like a charm the very first time. Thanks for for your input.