Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using transformer secondary windings
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 302 subscribers
  • Views 2096 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using transformer secondary windings

colporteur
colporteur over 4 years ago

image

Can I use both secondary windings to power separate loads?

 

I have a need for two 4.5VAC power supplies.

I have a transformer that is 9VAC with a center tap. I would like to connect one load to one 4.5VAC O/P and the other load to the other 4.5VAC. I'm assuming I can do this, provided I don't exceed the max current rating. It has been a long time since I have dabbled this low in analogue. I was looking for some reassurance or refresher.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago in reply to Jan Cumps +3
    Thanks JC for the reply. The AC loads are two small model railroad buildings that require 4.5VAC. It looks like they have some internal electronics to generate power for the few LEDS scatter around. It…
  • gdstew
    gdstew over 4 years ago +1
    As far as I can remember you can use a half wave rectifier on both output taps and the share the center tap as ground there is no problem with the circuits connecting to each other. Using half wave rectification…
  • colporteur
    colporteur over 4 years ago in reply to gdstew +1
    Only need the AC. I have no need for the rectifier stuff.
Parents
  • gdstew
    gdstew over 4 years ago

    As far as I can remember you can use a half wave rectifier on both output taps and the share the center tap as ground there is no

    problem with the circuits connecting to each other. Using half wave rectification will require that the cap on the diode output to be

    much larger to hold the voltage during the unused half wave to keep the ripple voltage to acceptable levels.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to gdstew

    Only need the AC. I have no need for the rectifier stuff.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 4 years ago in reply to colporteur

    You can still use the center tap as the common ground to both circuits. This is how the AC power in a US house works. There is a 240VAC CT step down transformer

    that supplies two 120VAC circuits to the breaker box, and both circuits are used to supply 240V where needed. The center tap from the transformer is connected to

    earth ground at the breaker box. It is also connected to the common (white) wire in the 120V AC outlets in the house.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 4 years ago in reply to colporteur

    You can still use the center tap as the common ground to both circuits. This is how the AC power in a US house works. There is a 240VAC CT step down transformer

    that supplies two 120VAC circuits to the breaker box, and both circuits are used to supply 240V where needed. The center tap from the transformer is connected to

    earth ground at the breaker box. It is also connected to the common (white) wire in the 120V AC outlets in the house.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 4 years ago in reply to gdstew

    Never thought of the 220VAC scenario. Fits perfect for what I am trying to do. Thanks for the insight. I will use it to explain it to the model railroaders.