Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17210 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello Nick;
    i'm using a current DAC from analog devices (AD5428) that did not work for me, 
    http://www.analog.com/en/digital-to-analog-converters/da-converters/ad5428/products/product.html
    i select DAC A and i put a load on Iout A but the potential is always zero, i doubt about using an amplifier before connecting the load directly to the IoutA, but i get nothing also, my ad5428 is mounted on a breadboard, and there is time diagram that i follow by using switch,
    thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello Nick;
    i'm using a current DAC from analog devices (AD5428) that did not work for me, 
    http://www.analog.com/en/digital-to-analog-converters/da-converters/ad5428/products/product.html
    i select DAC A and i put a load on Iout A but the potential is always zero, i doubt about using an amplifier before connecting the load directly to the IoutA, but i get nothing also, my ad5428 is mounted on a breadboard, and there is time diagram that i follow by using switch,
    thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor
    Without more circuit information it is difficult to know the exact nature of the problem. However, it does seem as though you have a low value resistive load at the output. Considering that the DAC as constructed per Figure 37 of the data sheet, we find that, with a load resistor between the output and some voltage Vterm, the general form of the output is:

     

              Vout = Vterm + [ (Vref – Vterm) * Load R ] /(Rdac + Load R)

     

    where Vterm is as described above, Vref is the DAC reference voltage, Load R is the resistance of your load and Rdac is a nominal 10k, with minimum and maximum of 8k and 12k, as described in the data sheet page 16. The above formula is valid for any value of Vterm between 0V (ground) and the DAC supply voltage.

     

    The probable reasons you are seeing no output include the following:

      Your load resistance is very low, Vterm is 0V and you are measuring the voltage output to ground or output to Vterm
      Vterm is the same as Vref and you are measuring a voltage across the load or the current through the load

     

    Please know that the output voltage of this type of DAC should always be maintained at 0V to get accurate current output, which is why all of the applications in the data sheet show the use of op-amps as current-to-voltage converters.

     

    I suggest that you look at the AD5410 to source a current. It has output current ranges of 0 to 20mA, 0 to 24mA and 4 to 20mA.

     

    If you want to sink a current, I suggest you try the DAC-08. It can sink up to 4mA as long as its output is always at least 5V above its negative supply.