Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17419 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago
    Can you help me with part numbers to make this http://www.rensu.net/sivut/RXL/SM/TTL-RS232.GIF .
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago
    Can you help me with part numbers to make this http://www.rensu.net/sivut/RXL/SM/TTL-RS232.GIF .
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nickgray
    nickgray over 16 years ago in reply to e14 Contributor
    I am sorry, but I am not sure just what kind of "help" you need because the part types are indicated on the schematic. U1 is a "7805" type linear regulator, U2 is a "MAX232", J2 is what is known as a "DB9" connector which is used for RS-232RS-232 interfaces and J1 appears to be a header to connect to whatever is sending and receiving data over the RS-232RS-232 port.

    The 7805 comes in TO-3, TO-220, TO-263 and SOT-223 packages. I believe that any of these packages would be satisfactory, but the SOT-223 and TO-263 packages MIGHT not handle the power requirements of this circuit (max 105mW) without care in how it is mounted. See the data sheet for proper mounting considerations. The TO-220 package should have no problems with power dissipation. Furthermore, I would prefer the LM340 because its specification shows a a little tighter tolerance on the output voltage. Data sheet is at http://www.national.com/ds/LM/LM340.pdf.

    The MAX232 was first introduced by Maxim Integrated Products, but is now available from other semiconductor manufacturers and is available in 16-pin plastic DOP and SOIC. C2 and C3 are used for the on-chip voltage multiplier to boost the +5V from the 7805 or LM340 to +12V and -12V. Data sheet is at http://datasheets.maxim-ic.com/en/ds/MAX220-MAX249.pdf.

    If none of this answers your questions, please clarify just what you need and I will try to provide your answers.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 16 years ago in reply to e14 Contributor
    I am sorry, but I am not sure just what kind of "help" you need because the part types are indicated on the schematic. U1 is a "7805" type linear regulator, U2 is a "MAX232", J2 is what is known as a "DB9" connector which is used for RS-232RS-232 interfaces and J1 appears to be a header to connect to whatever is sending and receiving data over the RS-232RS-232 port.

    The 7805 comes in TO-3, TO-220, TO-263 and SOT-223 packages. I believe that any of these packages would be satisfactory, but the SOT-223 and TO-263 packages MIGHT not handle the power requirements of this circuit (max 105mW) without care in how it is mounted. See the data sheet for proper mounting considerations. The TO-220 package should have no problems with power dissipation. Furthermore, I would prefer the LM340 because its specification shows a a little tighter tolerance on the output voltage. Data sheet is at http://www.national.com/ds/LM/LM340.pdf.

    The MAX232 was first introduced by Maxim Integrated Products, but is now available from other semiconductor manufacturers and is available in 16-pin plastic DOP and SOIC. C2 and C3 are used for the on-chip voltage multiplier to boost the +5V from the 7805 or LM340 to +12V and -12V. Data sheet is at http://datasheets.maxim-ic.com/en/ds/MAX220-MAX249.pdf.

    If none of this answers your questions, please clarify just what you need and I will try to provide your answers.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 16 years ago in reply to e14 Contributor
    I am sorry, but I am not sure just what kind of "help" you need because the part types are indicated on the schematic. U1 is a "7805" type linear regulator, U2 is a "MAX232", J2 is what is known as a "DB9" connector which is used for RS-232RS-232 interfaces and J1 appears to be a header to connect to whatever is sending and receiving data over the RS-232RS-232 port.

    The 7805 comes in TO-3, TO-220, TO-263 and SOT-223 packages. I believe that any of these packages would be satisfactory, but the SOT-223 and TO-263 packages MIGHT not handle the power requirements of this circuit (max 105mW) without care in how it is mounted. See the data sheet for proper mounting considerations. The TO-220 package should have no problems with power dissipation. Furthermore, I would prefer the LM340 because its specification shows a a little tighter tolerance on the output voltage. Data sheet is at http://www.national.com/ds/LM/LM340.pdf.

    The MAX232 was first introduced by Maxim Integrated Products, but is now available from other semiconductor manufacturers and is available in 16-pin plastic DOP and SOIC. C2 and C3 are used for the on-chip voltage multiplier to boost the +5V from the 7805 or LM340 to +12V and -12V. Data sheet is at http://datasheets.maxim-ic.com/en/ds/MAX220-MAX249.pdf.

    If none of this answers your questions, please clarify just what you need and I will try to provide your answers.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 16 years ago in reply to e14 Contributor
    I am sorry, but I am not sure just what kind of "help" you need because the part types are indicated on the schematic. U1 is a "7805" type linear regulator, U2 is a "MAX232", J2 is what is known as a "DB9" connector which is used for RS-232RS-232 interfaces and J1 appears to be a header to connect to whatever is sending and receiving data over the RS-232RS-232 port.

    The 7805 comes in TO-3, TO-220, TO-263 and SOT-223 packages. I believe that any of these packages would be satisfactory, but the SOT-223 and TO-263 packages MIGHT not handle the power requirements of this circuit (max 105mW) without care in how it is mounted. See the data sheet for proper mounting considerations. The TO-220 package should have no problems with power dissipation. Furthermore, I would prefer the LM340 because its specification shows a a little tighter tolerance on the output voltage. Data sheet is at http://www.national.com/ds/LM/LM340.pdf.

    The MAX232 was first introduced by Maxim Integrated Products, but is now available from other semiconductor manufacturers and is available in 16-pin plastic DOP and SOIC. C2 and C3 are used for the on-chip voltage multiplier to boost the +5V from the 7805 or LM340 to +12V and -12V. Data sheet is at http://datasheets.maxim-ic.com/en/ds/MAX220-MAX249.pdf.

    If none of this answers your questions, please clarify just what you need and I will try to provide your answers.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 16 years ago in reply to e14 Contributor
    I am sorry, but I am not sure just what kind of "help" you need because the part types are indicated on the schematic. U1 is a "7805" type linear regulator, U2 is a "MAX232", J2 is what is known as a "DB9" connector which is used for RS-232RS-232 interfaces and J1 appears to be a header to connect to whatever is sending and receiving data over the RS-232RS-232 port.

    The 7805 comes in TO-3, TO-220, TO-263 and SOT-223 packages. I believe that any of these packages would be satisfactory, but the SOT-223 and TO-263 packages MIGHT not handle the power requirements of this circuit (max 105mW) without care in how it is mounted. See the data sheet for proper mounting considerations. The TO-220 package should have no problems with power dissipation. Furthermore, I would prefer the LM340 because its specification shows a a little tighter tolerance on the output voltage. Data sheet is at http://www.national.com/ds/LM/LM340.pdf.

    The MAX232 was first introduced by Maxim Integrated Products, but is now available from other semiconductor manufacturers and is available in 16-pin plastic DOP and SOIC. C2 and C3 are used for the on-chip voltage multiplier to boost the +5V from the 7805 or LM340 to +12V and -12V. Data sheet is at http://datasheets.maxim-ic.com/en/ds/MAX220-MAX249.pdf.

    If none of this answers your questions, please clarify just what you need and I will try to provide your answers.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 16 years ago in reply to e14 Contributor
    I am sorry, but I am not sure just what kind of "help" you need because the part types are indicated on the schematic. U1 is a "7805" type linear regulator, U2 is a "MAX232", J2 is what is known as a "DB9" connector which is used for RS-232RS-232 interfaces and J1 appears to be a header to connect to whatever is sending and receiving data over the RS-232RS-232 port.

    The 7805 comes in TO-3, TO-220, TO-263 and SOT-223 packages. I believe that any of these packages would be satisfactory, but the SOT-223 and TO-263 packages MIGHT not handle the power requirements of this circuit (max 105mW) without care in how it is mounted. See the data sheet for proper mounting considerations. The TO-220 package should have no problems with power dissipation. Furthermore, I would prefer the LM340 because its specification shows a a little tighter tolerance on the output voltage. Data sheet is at http://www.national.com/ds/LM/LM340.pdf.