Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17419 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Nathan,

     

    Let me make clear from the beginning...I am not Nick :>)  I am sure he will reply with a well thought out answer.

     

    However, being in the audio business, your post caught my attention.

     

    My immediate response is to use an associative or content addressable memory.  There are not many simple AM or CAM devices on the market. Those that are one the market are more sophisticated and typically used in high speed search and pattern matching applications.

     

    Since you say you have only an 8 bit converter and need only 256 bits, one could take a small EPROM that had an 8 bit address bus and for each address location program the EPROM memory at that location with whatever HOH data you wanted instead the data at the A-D output.  For each possible A-D value, you could then have an alternative HOH value stored in EPROM memory which would be output to the digital amplifier instead.

     

    You would use a standard EPROM programmer for this task. 

     

    In operation, you would wire the EPROM to output data synchronously with the output rate of the A-D.  Depending upon the converter used, there should be an output synchronous with the 8-bit output.  That synchronous output would be used to enable the READ operation on the EPROM.  It would probably have to be delayed so that it would only cause the EPROM output after the A-D outputs were stable on the EPROM address lines. Otherwise, you might introduce data changes to the audio amplifier which would be basically interpreted as noise.  The delay sould be on the order of microseconds, not milliseconds.

     

    You could try this out on a bench setup, and if the HOH data were fairly consistent over a large group of listeners, you may be able to put the HOH data in a custom memory chip (if production volumes are high enough), or put it in one time programmable ROM, or even a small FPGA.

     

    Good Luck,

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Nathan,

     

    Let me make clear from the beginning...I am not Nick :>)  I am sure he will reply with a well thought out answer.

     

    However, being in the audio business, your post caught my attention.

     

    My immediate response is to use an associative or content addressable memory.  There are not many simple AM or CAM devices on the market. Those that are one the market are more sophisticated and typically used in high speed search and pattern matching applications.

     

    Since you say you have only an 8 bit converter and need only 256 bits, one could take a small EPROM that had an 8 bit address bus and for each address location program the EPROM memory at that location with whatever HOH data you wanted instead the data at the A-D output.  For each possible A-D value, you could then have an alternative HOH value stored in EPROM memory which would be output to the digital amplifier instead.

     

    You would use a standard EPROM programmer for this task. 

     

    In operation, you would wire the EPROM to output data synchronously with the output rate of the A-D.  Depending upon the converter used, there should be an output synchronous with the 8-bit output.  That synchronous output would be used to enable the READ operation on the EPROM.  It would probably have to be delayed so that it would only cause the EPROM output after the A-D outputs were stable on the EPROM address lines. Otherwise, you might introduce data changes to the audio amplifier which would be basically interpreted as noise.  The delay sould be on the order of microseconds, not milliseconds.

     

    You could try this out on a bench setup, and if the HOH data were fairly consistent over a large group of listeners, you may be able to put the HOH data in a custom memory chip (if production volumes are high enough), or put it in one time programmable ROM, or even a small FPGA.

     

    Good Luck,

    Ken