Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17179 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi!

    For an audio application, I am thinking about using the TI PCM1792ADB.PCM1792ADB. DAC. Its datasheet (http://focus.ti.com/general/docs/lit/getliterature.tsp?genericPartNumber=pcm1792a&fileType=pdf) suggests a schematic in Figure 36 (Page 35) for converting the differential current output to single-ended voltage output using NE5534NE5534 and LT1028 op-amps on +-15V rails.
    (a) Is it possible to reach a similar performance without the negative supply rail?
    (b) Would the  LTC6252 / LTC6253 op-amps run from 0V and 5V be a sensible choice, or should I use different op-amps?
    (c) Will I have to make larger changes in the schematic, or are the op-amps drop-in replaceable?

     

    Spida

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi!

    For an audio application, I am thinking about using the TI PCM1792ADB.PCM1792ADB. DAC. Its datasheet (http://focus.ti.com/general/docs/lit/getliterature.tsp?genericPartNumber=pcm1792a&fileType=pdf) suggests a schematic in Figure 36 (Page 35) for converting the differential current output to single-ended voltage output using NE5534NE5534 and LT1028 op-amps on +-15V rails.
    (a) Is it possible to reach a similar performance without the negative supply rail?
    (b) Would the  LTC6252 / LTC6253 op-amps run from 0V and 5V be a sensible choice, or should I use different op-amps?
    (c) Will I have to make larger changes in the schematic, or are the op-amps drop-in replaceable?

     

    Spida

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nickgray
    nickgray over 15 years ago in reply to e14 Contributor
    Hello Spida,

    Yes, it is possible to reach similar performance without a negative supply rail, but believe that 5V is insufficient voltage for this circuit because 2Vrms output of this circuit is the same as 5.66V peak-to-peak. However, if you use a rail-to-rail op-amps and 402 Ohms for the feedback resistors of U1 and U2, you can get about 1Vrms from the circuit. However, even rail-to-rail amplifiers will distort the signal as you approach the rails, so I am not sure that you can get the same performance with them.

    As a result of your and other questions I have seen over the years, I wrote a blog on doing this. Please see it at http://www.element-14.com/community/blogs/analog-by-nickgray/2010/12/01/going-from-bipolar-to-unipolar-supplies.

    - Nick Gray