Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17186 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    .  I am trying to design a solar positioning  system  to control the  movement of a panel useing the cn7485 comparator  I need a  4 bit analog  to  digital  converter   to feed the 7485

    THANK   YOU  .TIM   td1022@yahoo.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to e14 Contributor

    Hi Tim,

    In general, 4-bit ADCs (analog-to-digital converters are very high speed (hundreds of megasamples per second and higher) devices and expensive. I would look for an inexpensive 6-bit or 8-bit ADC and just use the 4 MSBs from it. This will be less costly than using an  ultra high speed 4-bit ADC. The reason that a really inexpensive ADC is adequate is because you will end up with more than enough accuracy for four bits and even the cheapest of today's 8-bit ADCs will perform well at the 4-bit level. The problem might be that today's loc speed, low cost ADCs generally come with serial output. This is to lower the packaging cost, which can be high with a parallel output. Here are some suggestions:

    From Analog Devices: AD7170BCPZ-REEL7AD7170BCPZ-REEL7, AD7478, AD7171BCPZ-REEL7AD7171BCPZ-REEL7, AD7468.

    From National Semiconductor: ADC081S021CIMF/NOPBADC081S021CIMF/NOPB

    From Texas lnstruments; TLC5510 (parallel output, twice the cost of those above)

    Having answered your question, I now offer what I think is a less costly solution. It certainly seems that you are considering a primaryly digital solution. I suggest an analog solution with two sensors placed within a fixture with two chambers side by side such that one light sensor is facing up in the bottom of each chamber. The chambers would be open only at the top and the side that is opposite from the other chamber. The output of the sensors would go to the "+" inputs of different analog voltage comparators (you can use a dual voltage comparator in a single package), Between the two sensors place a resistor, potentiometer and another resistor in series with each other. The two resistors connected directly to the sensor outputs could be 10 k-Ohms to 100 k-Ohms and the pot can be 50 k-Ohms to 1 Megohm. The arm of the pot and the "-" inputs of the two comparators are connected together. Between the output and the "+" input of each comparator put a 50K to 100K resistor for hysteresis to keep the comparators from oscillating.

    With the sun shining fully on both sensors, adjust the pot all the way to one end of its travel and confirm that one comparator output is high and the other is low. Adjust the pot all the way to the other end and confirm that the output conditions of both comparators have changed. If this does not happen, increase the value of the pot. Once you settle upon a pot value, adjust the pot to one side, again with light shining equally on both sensors. Then move the pot toward the center until one of the comparator outputs just barely changes state. Measure and record the voltage at the arm of the pot. Move the pot all the way to the other end of its travel and then move it back until the other comparator output just barely changes state. Measure and record the voltage at the arm of the pot. Determine the average of these two readings, then set the arm of the pot for that average voltage. Connect the comparator outputs to a system that will turn the positioning motor one direction when one of the comparators is high and the other low, and turn the motor in the other direction when the opposite is true for the two outputs. When the comparator outputs are the same, then the motor should not be driven. I will leave the design of the drive system to you.

    Good luck!

    Nick Gray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nickgray
    nickgray over 15 years ago in reply to e14 Contributor

    Hi Tim,

    In general, 4-bit ADCs (analog-to-digital converters are very high speed (hundreds of megasamples per second and higher) devices and expensive. I would look for an inexpensive 6-bit or 8-bit ADC and just use the 4 MSBs from it. This will be less costly than using an  ultra high speed 4-bit ADC. The reason that a really inexpensive ADC is adequate is because you will end up with more than enough accuracy for four bits and even the cheapest of today's 8-bit ADCs will perform well at the 4-bit level. The problem might be that today's loc speed, low cost ADCs generally come with serial output. This is to lower the packaging cost, which can be high with a parallel output. Here are some suggestions:

    From Analog Devices: AD7170BCPZ-REEL7AD7170BCPZ-REEL7, AD7478, AD7171BCPZ-REEL7AD7171BCPZ-REEL7, AD7468.

    From National Semiconductor: ADC081S021CIMF/NOPBADC081S021CIMF/NOPB

    From Texas lnstruments; TLC5510 (parallel output, twice the cost of those above)

    Having answered your question, I now offer what I think is a less costly solution. It certainly seems that you are considering a primaryly digital solution. I suggest an analog solution with two sensors placed within a fixture with two chambers side by side such that one light sensor is facing up in the bottom of each chamber. The chambers would be open only at the top and the side that is opposite from the other chamber. The output of the sensors would go to the "+" inputs of different analog voltage comparators (you can use a dual voltage comparator in a single package), Between the two sensors place a resistor, potentiometer and another resistor in series with each other. The two resistors connected directly to the sensor outputs could be 10 k-Ohms to 100 k-Ohms and the pot can be 50 k-Ohms to 1 Megohm. The arm of the pot and the "-" inputs of the two comparators are connected together. Between the output and the "+" input of each comparator put a 50K to 100K resistor for hysteresis to keep the comparators from oscillating.

    With the sun shining fully on both sensors, adjust the pot all the way to one end of its travel and confirm that one comparator output is high and the other is low. Adjust the pot all the way to the other end and confirm that the output conditions of both comparators have changed. If this does not happen, increase the value of the pot. Once you settle upon a pot value, adjust the pot to one side, again with light shining equally on both sensors. Then move the pot toward the center until one of the comparator outputs just barely changes state. Measure and record the voltage at the arm of the pot. Move the pot all the way to the other end of its travel and then move it back until the other comparator output just barely changes state. Measure and record the voltage at the arm of the pot. Determine the average of these two readings, then set the arm of the pot for that average voltage. Connect the comparator outputs to a system that will turn the positioning motor one direction when one of the comparators is high and the other low, and turn the motor in the other direction when the opposite is true for the two outputs. When the comparator outputs are the same, then the motor should not be driven. I will leave the design of the drive system to you.

    Good luck!

    Nick Gray