Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17213 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Nick,

     

    I have read the tutorial document you had previously linked to a user enquiring about analog switches.

     

    Perhaps you can help me understand something basic about the ADG419BZ analog switch. What is the maximum voltage that can be applied to the output pins (s1 and s2)? What would this information be listed under in the datasheet?

     

    Also, it says that the device can operate from a 12V single supply but can be remain functional to voltages as low as 5V. Does this mean I can apply 5V to the VDD pin?

     

    If you can help me on these points, I would be very grateful.


    Regards

     

    Rachel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Nick,

     

    I have read the tutorial document you had previously linked to a user enquiring about analog switches.

     

    Perhaps you can help me understand something basic about the ADG419BZ analog switch. What is the maximum voltage that can be applied to the output pins (s1 and s2)? What would this information be listed under in the datasheet?

     

    Also, it says that the device can operate from a 12V single supply but can be remain functional to voltages as low as 5V. Does this mean I can apply 5V to the VDD pin?

     

    If you can help me on these points, I would be very grateful.


    Regards

     

    Rachel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor

    Hi, Rachel –

    I am very happy to answer your  question on analog switches.

    The ADG419 is an analog switch from Analog Devices and is their version of the DG419 from Vishay Siliconix. The letters at the end of the device type indicate the type of package, temperature range and how the device is packaged (tape-and-reel, etc.).

    Most specifications for the “Operating Conditions” of electronic components can be found in the specification tables of the data sheet. However, analog switches often do not have input range on their data sheets. This is because it is assumed that the input can be anywhere within the negative and positive supply voltages of the product. Often the negative supply voltage is zero Volts. If you look at Figure 6 on page 7 of the ADG419 data sheet, you will note that, for a single supply, the curves show the “On” resistance from 0V to the voltage of the supply. This tells you that you can go to these limits. Figure 3 on the same page tells you that you allow the input voltage to go down to the negative supply voltage and up to the positive supply voltage. What may not be obvious from these graphs is that the input (or output) voltage is on the horizontal axis. VS is the voltage on either “S” input and VD is the voltage on the “D” input.

    Note that these figures indicate that the “on” resistance, which is the resistance between input and output, changes as the input voltage changes. This can lead to signal distortion if you are not careful. This is true of all analog switches.

    Yes, you can use this analog switch with a single 5V supply applied to the VDD pin, but from Figure 6 you will note that the “on” resistance that ranges between less than 60 Ohms to above 70 Ohms. This may or may not be a problem in your application. The Vishay Siliconix DG419 with a 5V supply has an “on” resistance that varies between a little over 30 Ohms to less than 50 Ohms, as seen in the plot at the top left of page 5 of that data sheet. The variation is larger than the Analog Devices’ product, but has a lower value. Which would be better for you will depend upon just what you are doing with it. If you are putting a fairly high quality AC signal through it (like audio, for example), I would prefer the analog device product because it has less variation (and percentage variation), so would give you less distortion (also, larger signals would mean more distortion). If you are passing only DC through it, I would prefer the Vishay Siliconix product because you would get less voltage drop across it.

    I do hope that this answers your question. Let me know if you need anything else.

     

    Nick