Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17238 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi

    I have a project that reads 4 air pressure sensors, performs some calculations and displays the values on 4 seven digit displays.

    To complete the project, I want to include a 6 position rotary selector so I can select different algorithms that the code can apply to the Analogue values coming from the sensors.

    The way I thought of doing this is to connect 5v to the Selector with different resistors on each of the 6 output pins. Then the Arduino would check the voltage to determine which position the selector is at.

    Problem is that I have used up all 6 analogue inputs.

    I guess I could use one of the free digital pins and use an analogue to digital converter but I don’t have a lot of space to be adding more boards. Is there some other way I can do this?

    Most of the digital pins are free.

    Thanks in advance

    Sam

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi

    I have a project that reads 4 air pressure sensors, performs some calculations and displays the values on 4 seven digit displays.

    To complete the project, I want to include a 6 position rotary selector so I can select different algorithms that the code can apply to the Analogue values coming from the sensors.

    The way I thought of doing this is to connect 5v to the Selector with different resistors on each of the 6 output pins. Then the Arduino would check the voltage to determine which position the selector is at.

    Problem is that I have used up all 6 analogue inputs.

    I guess I could use one of the free digital pins and use an analogue to digital converter but I don’t have a lot of space to be adding more boards. Is there some other way I can do this?

    Most of the digital pins are free.

    Thanks in advance

    Sam

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nickgray
    nickgray over 12 years ago in reply to e14 Contributor

    Hi, Sam –

    I am sorry that I did not see your question sooner, but I cave a couple of solutions for you. First, realize that it is not necessary to use a board level ADC as many ADC chips are easy to use. One example is the SPI output ADC081S021. I can suggest a complete circuit, if you need it.

    Another solution is to use a string of 12 resistors with 6 voltage comparators. I know of only one device with six voltage comparators in it and that is the LMV7231 from TI. However, there are a few quad voltage comparators available and you can use two of those. The arm of your selector switch would be connected to the non-inverting input of all voltage comparators. The series resistor string would have 13 nodes, numbered 0 through 12, with node 0 at ground and node 12 at perhaps 5 Volts. The even nodes 2 through 10 plus ground are each connected to separate pins of the rotary switch and the odd nodes are each connected to the inverting node of separate voltage comparators. As higher voltages are selected, more and more comparator outputs go high.

    Other topologies are possible, but I think these two provide the fewest components.

    Nick Gray