Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Signal conditioning chip for a single point load cell
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 339 subscribers
  • Views 914 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Signal conditioning chip for a single point load cell

e14 Contributor
e14 Contributor over 16 years ago
Hi.. i'm looking for a signal conditioning CHIP for converting the output of a single point load cell of 2mV/V to 0~10v. this chip must consist of a low pass filter which is to remove the noise ( high freq) and an amplifier to amplify the signal from 2mV to the range of 0~10V.Do you have any idea on this kind of chip? can i have the s/n of this chip? Thanks
  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 16 years ago

    You need a bit more spec before you can decide how to process the signal. For load cell signal the key parameters are usually noise, offset drift over temperature and gain drift over temperature. Undemanding applications can get away with 'scale on  a chip' solutions but good load cells outperform such chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 16 years ago in reply to michaelkellett

    Michael,

    You bring up a very good pooint. However, many people looking for load cell conditioning circuits or chips do not need all of the performance that the load cell will provide. I leave it to the user to decide if a given circuit or chip will provide the performance he/she needs. With the type of questions we have on this forum, there is generally no way to know all of the requirements any given person has. But your comment is a good one and I do appreciate it.

     

    - Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nickgray
    nickgray over 16 years ago in reply to michaelkellett

    Michael,

    You bring up a very good pooint. However, many people looking for load cell conditioning circuits or chips do not need all of the performance that the load cell will provide. I leave it to the user to decide if a given circuit or chip will provide the performance he/she needs. With the type of questions we have on this forum, there is generally no way to know all of the requirements any given person has. But your comment is a good one and I do appreciate it.

     

    - Nick