Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Signal conditioning chip for a single point load cell
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 339 subscribers
  • Views 892 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Signal conditioning chip for a single point load cell

e14 Contributor
e14 Contributor over 16 years ago
Hi.. i'm looking for a signal conditioning CHIP for converting the output of a single point load cell of 2mV/V to 0~10v. this chip must consist of a low pass filter which is to remove the noise ( high freq) and an amplifier to amplify the signal from 2mV to the range of 0~10V.Do you have any idea on this kind of chip? can i have the s/n of this chip? Thanks
  • Sign in to reply
  • Cancel
  • nickgray
    nickgray over 16 years ago

    I do not know of a chip that will give you up to 10V output, but there are chips that will give you a digital output. If you want 0 to 10V output, I would use an instrumentation amplifier. If you do not know how to use these amplifiers, tell me the load cell you are using and what voltage you want to power it from and I will try to help you with a circuit.

     

    Maxim Integrated Products makes two signal conditioning chips that I know of. They are the MAX1452 and the MAX1464. ZMD (http://www.zmdi.com) in Germany also has some signal conditioning chips for pressure sensors and load cells. Go to their web site and hover your mouse over the "Products" button and you will see 8 Sensor Signal Conditioner Products.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 16 years ago

    You need a bit more spec before you can decide how to process the signal. For load cell signal the key parameters are usually noise, offset drift over temperature and gain drift over temperature. Undemanding applications can get away with 'scale on  a chip' solutions but good load cells outperform such chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 15 years ago in reply to michaelkellett

    Michael,

    You bring up a very good pooint. However, many people looking for load cell conditioning circuits or chips do not need all of the performance that the load cell will provide. I leave it to the user to decide if a given circuit or chip will provide the performance he/she needs. With the type of questions we have on this forum, there is generally no way to know all of the requirements any given person has. But your comment is a good one and I do appreciate it.

     

    - Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Your load cell is a Wheatstone resistive bridge, if its a 4 wire you can use a differential A/D converter to convert that paramter. I'll leave the calculations up to you because you need to learn how to do that, but the ADS1248IPW.ADS1248IPW. http://focus.ti.com/docs/prod/folders/print/ads1248.html would be a good place to start if your going to put this on a board.