Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Multimeter? TENMA 72-6130 or FLUKE 106 any good?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 340 subscribers
  • Views 5802 views
  • Users 0 members are here
  • tenma
  • multimeter
  • fluke
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Multimeter? TENMA 72-6130 or FLUKE 106 any good?

mudz
mudz over 10 years ago

UPDATE 2(31/01/2016):
Finally, I went for FLUKE 115 as it was the only thing looked good at that price & I preferred quality over features this time. I purchased it for $100(Rs. 6729) here in India. Another DMM, I was also looking for was Mastec MS8218(50000 counts) but it was going over budget (at $165 or Rs. 11300). If I had money, I had gone for MS8218.
I have ordered(fluky 115) it today and waiting for its delivery. image

I will buy few more good multi meters(better than fluke 115) year.


UPDATE:
Kindly suggest me a good multi meter around $100 (+$20) range.

 

------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Hi,

All these years I managed to make my projects using$2 multi-meter I'm considering some better upgrade to that. Is TENMA  72-613072-6130 fine under $50 or FLUKE 107 or FLUKE 106 or TENMA 72-10395 will work fine?
Important specs:-

Voltage,

Current

resistance,

Frequency & duty cycle

continuity,


other bonus specs

capacitance,
Temperature

Transistor HFE

 

or is there something better below $50? Actually I have to buy few more components on a thin budget so I am cutting it down on multi-meter. Hopefully, I will buy another good one later this year but for now what do you suggest?

Thank you!

 

mudz

 

Update: to mention what I bought finally. :) Message was edited by: mudz

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +1
    Hi! Glad you asked before you purchased : ) Not sure on those little flukes - they are for general household use, not for engineers. I just checked the basics on those like resolution and if you can manually…
  • shabaz
    shabaz over 10 years ago in reply to mudz +1
    Hi! Uni-T are pretty awful (from experience). The Fluke 107 isn't appropriate either, it has a resolution of 1mA on the current range, which is unusable for electronics design. Why do you need frequency…
  • shabaz
    shabaz over 10 years ago in reply to mudz +1
    I think the Tenma one (72-7745) is about the right specification. The frequency measurement examples don't require a multimeter, so you could continue to use your existing multimeter until you have the…
Parents
  • mudz
    mudz over 10 years ago

    michaelkellett clem57 COMPACT
    Any suggestions?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to mudz

    Multimeters start from being a Dime a dozen to sophisticated, accurate and sensitive ones that cost tens of thousands of dollars or more.

    If you have minimal budget then I recommend that you have two cheap multimeters.

    An analog one and a digital one.

    The analog one is good for real time approximate readings for things like checking approximate resistances or checking switch operation.

    The digital one provides a bit more accuracy but with a slower response.

    Don't be fooled by meters that have both a digital display and analog meter display because the meter display is usually digital control as slow as snail.

     

    Having two multimeters allows you to simultaneously measure two readings such as reading current and voltage which I find quite handy.

     

    If you already have two multimeters (and power supply) then the next piece of equipment to obtain should be an Oscilloscope.

    This is because it gives you a great visualisation of what your DUT (device under test) is doing.

    It provides a continuous log of readings over time like so!

    image

     

    Remember when using this equipment - "SAFETY FIRST!"

    Obtain equipment with correct safety category.

     

    I'm actually hoping to get a Keithley  DMM7510DMM7510 or Keysight 34470A(with options but I'll have to win the lottery twice first

    Here's hoping!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 10 years ago in reply to mudz

    Multimeters start from being a Dime a dozen to sophisticated, accurate and sensitive ones that cost tens of thousands of dollars or more.

    If you have minimal budget then I recommend that you have two cheap multimeters.

    An analog one and a digital one.

    The analog one is good for real time approximate readings for things like checking approximate resistances or checking switch operation.

    The digital one provides a bit more accuracy but with a slower response.

    Don't be fooled by meters that have both a digital display and analog meter display because the meter display is usually digital control as slow as snail.

     

    Having two multimeters allows you to simultaneously measure two readings such as reading current and voltage which I find quite handy.

     

    If you already have two multimeters (and power supply) then the next piece of equipment to obtain should be an Oscilloscope.

    This is because it gives you a great visualisation of what your DUT (device under test) is doing.

    It provides a continuous log of readings over time like so!

    image

     

    Remember when using this equipment - "SAFETY FIRST!"

    Obtain equipment with correct safety category.

     

    I'm actually hoping to get a Keithley  DMM7510DMM7510 or Keysight 34470A(with options but I'll have to win the lottery twice first

    Here's hoping!