Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Ask the Expert: Fredy Klammsteiner - Sensor Application Expert
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 340 subscribers
  • Views 970 views
  • Users 0 members are here
  • experts
  • ask_an_expert
  • ask_the_expert
  • sensor
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Ask the Expert: Fredy Klammsteiner - Sensor Application Expert

patkelly
patkelly over 14 years ago

Fredy Klammsteiner is Custom Product Manager at Innovative Sensor Technologyimage

 

Fredy Klammsteiner is Custom Product Manager at Innovative Sensor Technology, consulting customers with special sensor application requirements in temperature, flow, humidity and conductivity. With a background as El. Eng. FH, Fredy joined IST in 2006 as Area Sales Manager for Eastern Europe, East Germany, Scandinavia and Russia and as Product Manager for TSic. In 2009 he became Head of Custom Products at IST.

 

Your title at IST?
Custom product manager

What is your education background?
El. Eng. FH

What are the areas of expertise within IST?
Consultancy of customers with special sensor application requirements, sales in several countries, product management of TSic sensor series, project management of custom sensors for temperature, flow, humidity, conductivity

And a short description of your work history?
2006 - 2009: Area Sales Manager Eastern Europe, East Germany, Scandinavia, Russia
2009 to date: Head of custom products

 

To ask Fredy a question reply to this discussion thread. Don't forget you will need to login or register to post your question

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    i have msp430fg4618 controller. i want to read hyt-221 sensor useing i2c.i interfaced sensor and useing IAR develop following code but its not work.NACK is coming from sensor.

    //******************************************************************************

    //   MSP430xG461x Demo - USCI_B0 I2C Master TX multiple bytes to MSP430 Slave

    //

    //   Description: This demo connects two MSP430's via the I2C bus. The master

    //   transmits to the slave. This is the master code. It continuously

    //   transmits an array of data and demonstrates how to implement an I2C

    //   master transmitter sending multiple bytes using the USCI_B0 TX interrupt.

    //   ACLK = 32kHz, MCLK = SMCLK = TACLK = BRCLK = 1MHz

    //

    //                                 /|\  /|\

    //                MSP430xG461x     10k  10k    MSP430xG461x

    //                    slave         |    |        master

    //              -----------------   |    |  -----------------

    //            -|XIN  P3.1/UCB0SDA|<-|---+->|P3.1/UCB0SDA  XIN|-

    //       32kHz |                 |  |      |                 | 32kHz

    //            -|XOUT             |  |      |             XOUT|-

    //             |     P3.2/UCB0SCL|<-+----->|P3.2/UCB0SCL     |

    //             |                 |         |                 |

    //

    //   Andreas Dannenberg/ M. Mitchell

    //   Texas Instruments Inc.

    //   October 2006

    //   Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A

    //******************************************************************************

    #include "msp430xG46x.h"

     

     

    volatile unsigned char k,d,t,*prxdata,s,txdatactr;                    

    volatile unsigned char data,rxdatactr,rxdata[5]={0,0,0,0,0},sdatactr;

    int i;

     

     

    void delay(int i)

    {

      while(i!=0)

      {

        i--;

      }

    }

    void main(void)

    {

      WDTCTL = WDTPW + WDTHOLD;

                     

    delay(60000);

     

     

      P3SEL |= 0x06;

      P2SEL |=0x00;

      P5SEL =0x00;

      P5DIR =0x02;

      P2DIR |= 0x06;

      P5OUT=0x00;

       UCB0CTL1 |= UCSWRST;                     

      UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;    

      UCB0CTL1 = UCSSEL_2 + UCSWRST;           

      UCB0BR0 = 10;                           

      UCB0BR1 = 0;

      UCB0I2CSA = 0x29;

    UCB0I2CIE =0x09;                        

      UCB0CTL1 &= ~UCSWRST;    

      P5OUT |=0x02;                                  

        

      while (1)

      {

         P2OUT=0x04;

        delay(60000);

        P2OUT=0x00;

        delay(60000);

        txdatactr=1;

        IE2 |= UCB0TXIE;

        k=1;

        __bis_SR_register(GIE);

        UCB0CTL1 |= UCTR + UCTXSTT;           

          while(k);    

          while (UCB0CTL1 & UCTXSTP);  

      

        P2OUT=0x04;

        delay(60000);

        P2OUT=0x00;

        delay(60000);

        t=1;

        rxdatactr=3;

        prxdata= &rxdata[0];

       

        IE2 |= UCB0RXIE;

         UCB0CTL1 &= ~UCTR;        

        UCB0CTL1 |= UCTXSTT;

        __bis_SR_register(CPUOFF + GIE);

       

         while (UCB0CTL1 & UCTXSTP);

         

    //UCB0CTL1 &= ~UCTXSTP;

      }

    }

     

     

    //------------------------------------------------------------------------------

    // The USCIAB0TX_ISR is structured such that it can be used to transmit any

    // number of bytes by pre-loading TXByteCtr with the byte count. Also, TXData

    // points to the next byte to transmit.

    //------------------------------------------------------------------------------

    #pragma vector = USCIAB0TX_VECTOR

    __interrupt void USCIAB0TX_ISR(void)

    {

      if(k==1)

      {

                if(txdatactr)

              {

                UCB0TXBUF=0x28;

                txdatactr--;

              }

            else

              {

      

                   UCB0CTL1 |= UCTXSTP;

                   //UCB0CTL1 &= ~UCTXSTT;

                   IFG2 &= ~UCB0TXIFG;

                   IE2 &= ~UCB0TXIE;

                   k=0;

                    //__bic_SR_register_on_exit(CPUOFF);

              }

     

      }

     

     

       if(t==1)

      {

      if (rxdatactr)                           

      {

      

       *prxdata=UCB0RXBUF;

       if((IFG2 & UCB0RXIFG)==0)

        {

          P5OUT |=0x02;

        }

     

       if(rxdatactr==1)

       {

        UCB0CTL1 |= UCTXSTP;

       }

        rxdatactr--;

        prxdata++;

      }

      else

      {

        *prxdata=UCB0RXBUF;

        // UCB0CTL1 |= UCTXSTP;          

       IE2 &= ~UCB0RXIE;

        t=0;

        __bic_SR_register_on_exit(CPUOFF);     

      }

      }

     

     

     

     

     

    }

     

     

    #pragma vector=USCIAB0RX_VECTOR

    __interrupt void USCIA0RX_ISR (void)

    {

      if((UCB0STAT && UCNACKIFG)==1)

      {

        P5OUT =0x00;

        UCB0STAT &=~UCNACKIFG;

      }

     

      if((UCB0STAT & UCALIFG)==1)

      {

        P5OUT |=0x00;

      }

    }         

     

     

     

     

     

    so plz help me///////

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fredy_Klammsteiner
    Fredy_Klammsteiner over 13 years ago in reply to e14 Contributor

    Dear karan patel

    Could you please send this request to my email address fredy.klammsteiner@ist-ag.com. I will forward it to our responsible person at IST AG.

     

    Thanks and best regards

     

    Fredy Klammsteiner

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fredy_Klammsteiner
    Fredy_Klammsteiner over 13 years ago in reply to e14 Contributor

    Dear karan patel

    Could you please send this request to my email address fredy.klammsteiner@ist-ag.com. I will forward it to our responsible person at IST AG.

     

    Thanks and best regards

     

    Fredy Klammsteiner