Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Do you have a question on PCB Fabrication? Ask our Expert, Nolan Johnson
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 341 subscribers
  • Views 3248 views
  • Users 0 members are here
  • sunstone_circuits
  • element14
  • expert
  • nolan
  • sunstone
  • pcb
  • pcb_fabrication
  • questions
  • Design
  • experience
  • engineering
  • ask
  • solution
  • johnson
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Do you have a question on PCB Fabrication? Ask our Expert, Nolan Johnson

e14 Contributor
e14 Contributor over 14 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about PCB Prototyping in the element14 Community PCB Prototyping group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Nolan Johnson

Nolan Johnson knows his way around CAD tools, and circuit board manufacturing. Having started his career as a CAD tool programmer, with over seven years at Sunstone Circuits, and more than twenty years in IC & PCB manufacturing, Nolan can help with design workflow issues and Manufacturing concerns for your PCB design work.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I'm a postgraduate student at the Indian Institute of Astrophysics, Bangalore, India. I'm working on a 6- chaannel photodiode amplifier, which will be used for site surveys for a new telescope coming up in India.

     

    A dual JFET opamp (LT1464) powered by ±15V supply is used to amplify the signals from a very sensitive photodiode (Thorlabs FDS1010) In the first stage, the current in the range of nanoamperes from the photodiode is converted to desirable volt range by a resistance of 9.1MΩ.


    Thereafter, DC and AC components of the signal are separated and given different amplification coefficients with the second stage, along with another low pass filter that eliminates all frequencies above 400 Hz. AC component of the signal is amplified by 110 times, while the DC is amplified by 2 times so as to bring out the scintillations from what would have been a DC dominated signal. A high pass filter is also integrated into the circuit to only admit all frequencies over 0.1 Hz. Necessity of clean power requires appropriate smoothening capacitors, to be connected across the power supply of the amplifier

     

    image

    With the current circuit configuration, the circuit tends to oscillate giving an output sinusoidal signal of less than 15V amplitude, without the application of any signal. According to Fig, it’s giving a sinusoidal signal of about 10-12V with NO DC offset, and a frequency of 564Hz in the absence of light from the LED (or for that matter, any light at all). Even when the photodiode was disconnected, the oscillations were still present, as shown in the figure

     

    image

    Following is the PCB layout

     

    image

    After reading more about PCB design, I found that the PCB was full of parasitic capacitances and there was plenty of crosstalk between the output of the six channels. So I decided to separate all the channels and adopt a better PCB design

     

    I'm making another board after reading through some PCB guidelines. I'm populating it only with SMD Resistors and caps (hopefully reducing the noise) and giving a proper ground and power plane. So, can you tell me whether there's any problem with this design before I give it for fabrication?

     

    image

    Following is the PCB design without the ground plane (for better visibility of the layout)

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    i want to design a self generating emf device without using any external voltage source ..

    please upload the circuit diagram along with the components name..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    i want to design a self generating emf device without using any external voltage source ..

    please upload the circuit diagram along with the components name..