Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum help with the flow sensor FS5
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 324 subscribers
  • Views 4229 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

help with the flow sensor FS5

Former Member
Former Member over 12 years ago

hi please i need help how to use my flow sensor FS5.

would like to measure flow of gas so i bought the FS5 but now i am reading the datasheet that i download from the webside but its not helping.

if anyone have use it befor can i have your circuit diagram please.

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +2
    Hi Leonel, A reference circuit is included in the data sheet: http://www.farnell.com/datasheets/484569.pdf You may need to reduce or offset the output voltage. Here is a link to an example: http://dl.dropboxusercontent…
  • dougw
    dougw over 12 years ago in reply to Former Member +2
    Hi Leonel, The sensor includes the heater (Rs is the Sensor Resistance and RH is the heater resistance in the circuit - both of these resistors are stuck together as part of the sensor you have). One wire…
  • Former Member
    Former Member over 12 years ago in reply to dougw +1
    hi Doug Thanks for your response. I saw the 2nd link in your response.I can see circuit diagram its exactly something like that that am looking for but have a concern: Its written sensor is it the FS5…
Parents
  • dougw
    dougw over 12 years ago

    Hi Leonel,

    A reference circuit is included in the data sheet:

    http://www.farnell.com/datasheets/484569.pdf

    You may need to reduce or offset the output voltage. Here is a link to an example:

    http://dl.dropboxusercontent.com/u/7549930/aaSchematic2-diffAmp.png

    and a discussion:

    output - arduino thermal anemometer - Electrical Engineering Stack Exchange

    If you cannot build it, you might be able to use the evaluation module from Farnel:

    160.00001 - IST INNOVATIVE SENSOR TECHNOLOGY - EVALUATION BOARD, FOR FS5 FLOW | Farnell UK

    http://www.farnell.com/datasheets/1702754.pdf

     

    Doug

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to dougw

    hi Doug

    Thanks for your response.

    I saw the 2nd link in your response.I can  see circuit diagram its exactly something like that that am looking for but have a concern:

    Its written sensor is it the FS5? and see heater as a block do need to buy a heater also? or its just the name of that leg of the sensor.

    Please be sore explicite please

    Waiting to hear from you.

    Leonel

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 12 years ago in reply to Former Member

    Hi,

    When you connect it up, what voltage is on each pin of the transistor?

    And each pin of each op-amp?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to dougw

    hi,sorry for the late response but apparently i am using the FS1 not FS5 can i use the same circuit. when i look at the datasheet of the FS1 there is a circuit on it different to the FS5. But on that circuit those resistors doesn't have value.

    please help

     

    leonel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 11 years ago in reply to Former Member

    The FS5 circuit should work fine for the FS1 sensor.

    With a 12 V supply, the heater won't draw more than 120 mA, so any battery should be adequate.

    If you measure all the voltages on the transistor and op-amp, we could help diagnose the issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to dougw

    hi,

    here are the measurement on the voltage on the transistor : pin1 and pin2 = 0.6Vdc

    on the oscilloscope i can see a waveform that its moving as i change the flow of the gas that i am sending to the sensor. but i have to reduce the volt per division to the smaller one to see that change.

    I don't know if that its just noise or its the signal that i am suposse to see and i have to filter it.

     

    Please guide me

     

    leonel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 11 years ago in reply to Former Member

    The signal should not change quickly - if it is changing rapidly, then it is most likely noise.

    The base of the transistor, which is connected to the output of the op-amp, should be  about .7 volts higher than the transistor emitter, which is connected to the resistor bridge.

    It looks like the emitter voltage should vary between about 5 volts and 7.5 volts depending on the flow rate (temperature).

    From your description of the voltages, it sounds like the voltage at the + input of the op-amp is too low. check to see that all resistors have the correct values and that the sensor and heater pins have not been reversed.

    What are the voltages on the input and output pins of the first op-amp?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to dougw

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • saeed.lanjekar
    saeed.lanjekar over 7 years ago in reply to dougw

    Dear Douglas,

     

    In 5 pin opamp, what is the part number of it?

    Why 2 pins are not connected which is used for operations?

    Your early reply highly appreciated

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to Former Member

    Air velocity is not linearly proportional to output voltage. You would need to calibrate against a known measurement method.

    The curve will look something like this one:

    http://www.farnell.com/datasheets/484569.pdf?COM=Discussions

     

    I think k is the thermal conductivity of air:

    https://www.engineeringtoolbox.com/air-properties-d_156.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to saeed.lanjekar

    In a 5 pin op-amp 2 pins are for power (supply voltage and ground)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago in reply to saeed.lanjekar

    In a 5 pin op-amp 2 pins are for power (supply voltage and ground)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data