Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum help with the flow sensor FS5
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 316 subscribers
  • Views 3837 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

help with the flow sensor FS5

Former Member
Former Member over 11 years ago

hi please i need help how to use my flow sensor FS5.

would like to measure flow of gas so i bought the FS5 but now i am reading the datasheet that i download from the webside but its not helping.

if anyone have use it befor can i have your circuit diagram please.

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago +2
    Hi Leonel, A reference circuit is included in the data sheet: http://www.farnell.com/datasheets/484569.pdf You may need to reduce or offset the output voltage. Here is a link to an example: http://dl.dropboxusercontent…
  • dougw
    dougw over 11 years ago in reply to Former Member +2
    Hi Leonel, The sensor includes the heater (Rs is the Sensor Resistance and RH is the heater resistance in the circuit - both of these resistors are stuck together as part of the sensor you have). One wire…
  • Former Member
    Former Member over 11 years ago in reply to dougw +1
    hi Doug Thanks for your response. I saw the 2nd link in your response.I can see circuit diagram its exactly something like that that am looking for but have a concern: Its written sensor is it the FS5…
  • dougw
    dougw over 11 years ago in reply to Former Member

    The signal should not change quickly - if it is changing rapidly, then it is most likely noise.

    The base of the transistor, which is connected to the output of the op-amp, should be  about .7 volts higher than the transistor emitter, which is connected to the resistor bridge.

    It looks like the emitter voltage should vary between about 5 volts and 7.5 volts depending on the flow rate (temperature).

    From your description of the voltages, it sounds like the voltage at the + input of the op-amp is too low. check to see that all resistors have the correct values and that the sensor and heater pins have not been reversed.

    What are the voltages on the input and output pins of the first op-amp?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to dougw

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago

    Referrng to FS5A flo sensor i have followng queries

    1) i fitted fs5A flow sensor in a 12.5mm pipe(inner diameter) 6 feet in length.i opened valve and air flow started flowng through pipe.i read 6 volts at output of cicuit (evaluation board circuit). Now from this 6 volt at at output how can i calculate air velocity at 25 C temperature? Any relation?

    2) secndly using king's law what is value of  "k" in that kings law with units

    Anyone help me please i will be grateful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mai109
    mai109 over 8 years ago

    Hi,

     

    I have a stupid question. Is the FS5 sensor supposed to be mounted perpendicular to or parallel with the direction of airflow?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago in reply to mai109

    Long thin edge facing the flow (perpendicular to the flow vector)  - do not block the flow when mounting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • saeed.lanjekar
    saeed.lanjekar over 7 years ago in reply to dougw

    Dear Douglas,

     

    In 5 pin opamp, what is the part number of it?

    Why 2 pins are not connected which is used for operations?

    Your early reply highly appreciated

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to Former Member

    Air velocity is not linearly proportional to output voltage. You would need to calibrate against a known measurement method.

    The curve will look something like this one:

    http://www.farnell.com/datasheets/484569.pdf?COM=Discussions

     

    I think k is the thermal conductivity of air:

    https://www.engineeringtoolbox.com/air-properties-d_156.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>