Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is an easy free way to convert CAD drawings to useable Gcode?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 339 subscribers
  • Views 1918 views
  • Users 0 members are here
  • cnc
  • arduino
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is an easy free way to convert CAD drawings to useable Gcode?

e14 Contributor
e14 Contributor over 12 years ago

Currently the biggest issue I'm having in this planning phase of making a arduino powered CNC mill is finding a good (freeware/shareware) way of converting my CAD files to usable Gcode. From everything I have read the easiest way to do this is to first run a .obj file through a CAM software and then interpret that into Gcode. Does anyone know of a good way to do this, I use autodesk Inventor to do all my drawings? I also have access to solid works while on campus, but I'm pretty sure both programs can output all the same file types. Anyways thanks for the help and updates to follow as I make progress.

  • Sign in to reply
  • Cancel
Parents
  • Nate1616
    Nate1616 over 12 years ago

    Hello Chris,

    The way most 3d printer users do it is to export out a stl file from your modeling software and download slicing software such as Slic3r Slic3r - G-code generator for 3D printers or Repetier Host Repetier-Host Documentation | Repetier Software just to name a few.  These 2 are free for download.  From there you can export out a gcode file.  Just remember these are made for printers so some mods will have to be made.   I would also check out this link GCODE Generators - ReplicatorG.  Let me know if you have any questions.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Nate1616

    Would those programs work for a CNC mill as well or are there different programs for that and 3D-printers, because in the long run I plan to also setup a swapable extruder head. Having a single software setup and only having to change out a router head to an extruder to convert between a CNC router/mill to a 3d printer would be ideal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 12 years ago in reply to e14 Contributor

    Yes, Slic3r has a setting for Mach3/EMC or "No Extrusion" for others besides Mach3 .

    image

    The last link I attached on the earlier post has some gcode generators specifically for CNC machines but both will work.  You will have to play with the settings to get the most out of you machine.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Nate1616
    Nate1616 over 12 years ago in reply to e14 Contributor

    Yes, Slic3r has a setting for Mach3/EMC or "No Extrusion" for others besides Mach3 .

    image

    The last link I attached on the earlier post has some gcode generators specifically for CNC machines but both will work.  You will have to play with the settings to get the most out of you machine.

     

    Nate