Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for way to switch 8 pins at once, either mechanically or low-powered electronics
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 339 subscribers
  • Views 3967 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for way to switch 8 pins at once, either mechanically or low-powered electronics

e14 Contributor
e14 Contributor over 11 years ago

Hi!

 

I'm building a mouse/joystick switch for use with old Atari/Amiga 16-bit computers. On these computers, joystick port 0 double as a mouse port, so if you want to play two-player games you have to swap the mouse for a joystick, which is a hassle (especially so on the Atari ST, where the port is underneath the machine). So a little box where you'd connect both mouse and joystick and switch to choose one of them would be helpful.

 

What I need is a way to switch 8 of the pins at once, either using a DPDT-style switch or something like a couple of 4066's.

 

However, the 4066's need power (of which I can draw only miniscule amounts from the port's 5V pin), and I simply can't find any suitable 8-pole mechanical switchers, probably because I'm not using the right search words.

 

A latching push button would be a nice mechanical solution, but even better would be a switch where it'd be immediately obvious which device is active, like a slider or a toggle switch.

 

 

Thanks in advance,

 

Per.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 11 years ago +1 suggested
    Hey, this is the first time that I can recommend the same IC in two different questions: SN74CBT16245DGGR: 16-Bit FET Bus that can switch two groups of 8 pins. Very fast. (I also recommended it for another…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Jan Cumps +1
    Thanks for the reply! That little guy (well, IC...) looks great, but I'm honestly not sure my soldering skills are up to it. But no, I didn't mention my beginner status, so how could you have known? But…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to jw0752 +1
    Wow, I would never have expected that, but I would not be so sure about the eBay specials
Parents
  • Jan Cumps
    0 Jan Cumps over 11 years ago

    Hey, this is the first time that I can recommend the same IC in two different questions:

    SN74CBT16245DGGR: 16-Bit FET Bus that can switch two groups of 8 pins. Very fast.

     

    (I also recommended it for another purpose in this discussion: TTL to CMOS protection / recommendation).


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Jan Cumps

    Thanks for the reply!

     

    That little guy (well, IC...) looks great, but I'm honestly not sure my soldering skills are up to it. But no, I didn't mention my beginner status, so how could you have known?

     

    But I might order one anyway and mount that scary hook-like tip on my Hakko just for fun! :-)

     

    Thanks for your help, I appreciate it!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    you can get break out boards for chips like that too, this way you can plug it into a bread board for prototyping

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    you can get break out boards for chips like that too, this way you can plug it into a bread board for prototyping

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Oooh, I didn't even consider that. I'll look for those too, thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to Robert Peter Oakes

    ... and it is solderable. One of the first SMD exercises I did was this IC (the first was an OPA2170 - SOIC-8. The SN74CBT16245DGGR is TSSOP-48).

    With paste and hot air it works rather well. SMD isn't that hard for these types of packages).

     

    Result:

    , image