Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Digital PI (Pulse Induction) metal detector.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 304 subscribers
  • Views 2013 views
  • Users 0 members are here
  • analog-to-digital
  • microcontrollers
  • metal
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Digital PI (Pulse Induction) metal detector.

Former Member
Former Member over 10 years ago

I want to build a digital PI (Pulse Induction) metal detector. Which components may be the best for this? I think I'll need a fast and precise AD converter and a fast micro controller to measure the voltage decay and then compare with a normal curve without metal present. ¿Am I in the right way?

Thanks in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago in reply to bobalexander +1
    I think that for the OP, PI means Pulse Induction not RaspberryPi. But never mind - the board you suggest is quite nice but based on an older STM32 processor which can't convert as fast as some of the…
  • bobalexander
    bobalexander over 10 years ago in reply to michaelkellett +1
    Good point - I completely missed that! I was under the impression that Pulse Induction is not a great option as you can never discriminate out iron. Perhaps that is what the OP is wanting to detect though…
Parents
  • bobalexander
    0 bobalexander over 10 years ago

    You could add a ARMinARM board if you are wanting to utilize the Pi as some kind of interface:

    onandoffables / hardware / arminarm / board

    The  STM32 ARM Cortex-M3 microcontroller 'backpack' would let you perform all the signal sensing and low level processing just passing off data to the Pi...

     

    Most metal detectors utilize a VLF transmitter and receiver to detect the presence of a metal.

    They then discriminate between ferrous and non-ferrous materials based on the phase shift of the returned signal. This allows you to tell if the metal you are detecting is a rusty old nail or a gold coin as each type of metal will shift the phase of the bounced signal differently.

     

    Here is a basic overview:

    http://www.thomasathomas.com/Metal_detectors_work.htm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to bobalexander

    I think that for the OP,  PI means Pulse Induction not RaspberryPi.

    But never mind -  the board you suggest is quite nice but based on an older STM32 processor which can't convert as fast as some of the more recent parts.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to bobalexander

    I think that for the OP,  PI means Pulse Induction not RaspberryPi.

    But never mind -  the board you suggest is quite nice but based on an older STM32 processor which can't convert as fast as some of the more recent parts.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bobalexander
    0 bobalexander over 10 years ago in reply to michaelkellett

    Good point - I completely missed that!

    I was under the impression that Pulse Induction is not a great option as you can never discriminate out iron.

    Perhaps that is what the OP is wanting to detect though...

     

    Good call on the older STM32 - I didn't even think about it not being fast enough for processing signals in the kHz range.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to michaelkellett

    Yes, PI stands for Pulse Induction, that's the reason why I need fast measurement, see the curve in the figure: